Hi TI-team
I confirmed the "Voltage-Level Translation With the LSF Family"
There is the following sentence on P.2.
Remember that the LSF device acts as a passive switch when the input signal is below Vref_A – 0.5 V.
Does this mean that the Vgs (th) of the internal FET is 0.5V ?
Is it not necessary to consider the variation of 0.5V ?
Is the input from the VinB side correct with the recognition that it is Vref_A-0.5 ?
Best Regards,
Koji Hayashi