This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC2G14-Q1: VIH & VIL minimum and maximum value calculate

Part Number: SN74LVC2G14-Q1

Hello,

I'm using the IC for relaxation oscillator, and I want to calculate the tolerance of my circuit. 

Operate temperature is -40 degrees to 125 degrees

Operate VCC = 4.9V to 5.1V, 

so is there any formula or curve relation of temperature with VIH and VIL?

and How is the minimum and maximum value definition? VCC tolerance or Temperature

My calculation is in the figure shows that there have the same value in minimum value in -40 degrees to 85 degrees & -40 degrees to 125 degrees

so I assume the minimum value is in -40 degrees and maximum value in 85 degrees and 125 degrees, and using interpolation to get the correspond value in different VCC

Thanks for apply.