Other Parts Discussed in Thread: SN74LVC2G14-Q1
Hello,
Kindly review the attached design using SN74LVC1G14QDCKRQ1
Thanks,
Melbin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Kindly review the attached design using SN74LVC1G14QDCKRQ1
Thanks,
Melbin
Hello,
We are working on a project with SN74LVC1G14QDCKRQ1 in it.
Kindly review the attached schematics and let me know the review comments.
Hi Melbin,
Thanks for the opportunity to review your schematics.
It looks like you're using the SN74LVC14-Q1 to invert two signals.
The parts that I can see on the schematic are fine.
The ST inputs should handle pretty much any signal you put in, however I can't see the input signals or output load, so I can't really comment on those besides saying keeping the input signals fast and near the rails will reduce power consumption, and the keeping the outputs lightly loaded will improve performance.
Hey Melbin,
The current circuit is fine. You could also just use the SN74LVC2G14-Q1.
Hey Melbin,
I don't see any issues.
Note that I can't see details regarding the load or input signals, so I can't comment on those.
Melbin,
I noticed that you have already posted this. In an effort to consolidate posts on E2E, I have merged the threads.
Best,
Danny