This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN10KHT5541: Is SN10KHT5541 fit for the requirement

Part Number: SN10KHT5541
Other Parts Discussed in Thread: LSF0108, TXB0108, TXS0108E, SN74AXC8T245

Hi team,

I searched from TI store and found part. could you help check if the part fit the requirement below? If not, can you advise one?

"

1.8V  to  3.3V  voltage-level translator

8-bit

Max 100MHz

Bidirectional

"

  • Hi,

    If you're looking for a voltage translator that will automatically translate bidirectional signals (such as I2C), the LSF0108, TXB0108, or the TXS0108E (for open drain applications) are great choices.

    If you're looking for something that can be controlled (has a DIR pin to pick the direction signals will travel) the SN74AXC8T245 is a good choice.

    Thanks!

    Chad Crosby