Hello,
This question may be already answered on this forum, but I haven't seen it: On the SN74AVC1T45 datasheet, there is two information that seems not fitting together:
1) Page 2: "This device is fully specified for partial-power-down applications using I off . The I off circuitry disables the outputs, preventing damaging current backflow through the device when it is powered down. The VCC isolation feature ensures that if either V CC input is at GND, then both ports are in the high-impedance state."
2) Page 9: "A proper power-up sequence always should be followed to avoid excessive supply current, bus contention, oscillations, or other anomalies. To guard against such power-up problems, take the following precautions:
1. Connect ground before any supply voltage is applied.
2. Power up VCCA .
3. VCCB can be ramped up along with or after VCCA"
My questions are:
- if the device can be used for partial power down and having either VCC input at GND, why is there a recommanded power up sequence?
- I found the same Ioff feature in the SN74AVC4T234 datasheet, but without the power up recommandation. Why?
Regards,
Thibault