This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LV14A: Equivalent circuit

Part Number: SN74LV14A

Hi

Do you have the equivalent circuit of this device or this family device of input pin?

I found a information of LVC series as following.

http://www.ti.com/lit/an/scba011/scba011.pdf

Can I use this for SN74LV?

Regards,

Koji Hamamoto

  • Hello Koji-san,

    The LV and LVC families are not the same process, so there are some differences. I would not refer you to the document you attached for the LV family.

    Since you are referring to the inputs of the device I am wondering if you are concerned with the actual structure of the inputs or the clamp diode structure, so I will address both below.

    The inputs are standard schmitt trigger high impedance inputs and for this device there is a negative clamping diode from gnd, but there is no positive clamping diode to VCC, so the inputs are overvoltage tolerant.

    I would also refer you to Question 2 as part of our Input Parameters section in our Logic FAQ.
    e2e.ti.com/.../3537.02-input-parameters

    Best,
    Michael