Other Parts Discussed in Thread: SN74AXC4T774
Hi Team,
My customer is working with the TXB0104 level shifter for SPI in a new design. In this case the VCCB rail is switched on and off periodically while the VCCA rail is always on. The OE pin is connected to a voltage divider connected to VCCB. The voltage divider shifts VCCB (3.3V) to the VCCA voltage level (1.8V).
In the static "ON" case the design obeys the requirement that VCCB (3.3V) > VCCA (1.8V).
They saw the note in section 10 in the TXB0104 datasheet that suggests that the device is protected during power-up even if VCCB < VCCA. Would that protection be sufficient in the case where VCCB powers up and down multiple times?
What type of failure modes might we expect to see, if not?
Is there any sort of undervoltage protection on the VCCA/VCCB rails, if there were to be a slow ramp down on the VCCB side?
Thanks!
Mitchell