Hello, I want to use SN74LVC1G11 connecting to an output with voltage higher than 5.5V. Does the SN74LVC1G11 has current sinking capability? If I place a current-limiting resistor, could I have an entering current when output voltage is high?
If so, which is the maximum sinking current? Is it 50 mA (35 mA nominal)?
Thanks!