This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TXB0108: OE Pin Treatment Confirmation

Intellectual 1480 points

Replies: 3

Views: 32

Part Number: TXB0108

Hi team,

I'd like to confirm the customer use case is okay or not.

Could you please check the questions below?

1: Is it okay to add a reset circuit connecting OE?

2: Is it okay to connect OE to Vcca directly?

Best Regards,

Kazuki Kitajima

  • 1. Yes

    2. Pulling OE down during power up ensures that the I/O pins are in the high-impedance state. If you do not care about the state of the I/Os during power up, then you can connect OE directly to VCC.

  • In reply to Clemens Ladisch:

    Hey Kazuki,

    I'd like to add to Clemens' first answer assuming you are talking about an RC delay: Technically, the answer is yes as long as you don't violate the input transition rate spec, but this will likely be impossible if you directly connect the RC. You will need an additional schmitt-trigger buffer to handle the slow transition.

    Check out our new AXC family of Voltage Translators! 

    Watch the Introduction to AXC Family to find out more about the family.

  • In reply to Dylan Hubbard:

    Hi Dylan-san, Clemens-san,

    Thank you for your reply.

    Understood.

    Best Regards,

    Kazuki Kitajima

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.