Hi Team,
My customer is trying to use SN74LVC2T45DUC.
They noticed a large leak current on the board they created.
I understand that when DIR = VCCA, VCCA = 3.3V, VCCB = 3.3V, A1 = 0V, A2 = 0V, then ΔIccA = max.50uA.
What is the value(typ.) at Ta=25 ℃?
In 11.2 Layout Example, the DIR pin is connected to VCCA via a resistor.
The customer is not connecting through a resistor, is it related to the leak current?
Is there a recommended resistance value?
Best Regards,
Kenji