Hi,
I am using RM57 bank 0 for bootloader and bank 1 for main application.
Linker command settings of my bootloader:
MEMORY
{
VECTORS (X) : origin=0x00000000 length=0x00000020
FLASH0 (RX) : origin=0x00000020 length=0x001fffe0
FLASH1 (RX) : origin=0x00200000 length=0x00200000
STACKS (RW) : origin=0x08000000 length=0x00001500
RAM
(RW) : origin=0x08001500 length=0x0007eb00
}
SECTIONS
{
.intvecs : {} > VECTORS
.text > FLASH0
.
const
> FLASH0
.cinit > FLASH0
.pinit > FLASH0
.bss > RAM
.data > RAM
.sysmem > RAM
}
Linker command settings of my main application:
MEMORY
{
VECTORS (X) : origin=0x00200000 length=0x00000020
FLASH1 (RX) : origin=0x00200020 length=0x001fffe0
STACKS (RW) : origin=0x08000000 length=0x00001500
RAM
(RW) : origin=0x08001500 length=0x0007eb00
}
SECTIONS
{
.intvecs : {} > VECTORS
.text > FLASH1
.
const
> FLASH1
.cinit > FLASH1
.pinit > FLASH1
.bss > RAM
.data > RAM
.sysmem > RAM
}
Problem : when i program and debug the main application code it is working fine and executing from 0x00200000 but during debugging if i did system reset then it is pointing to address 0x00000000 and showing undefined entry and halting there.
Kindly suggest me any other changes do i need to do ? or any mistakes above