This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RM57L843: Bootloader vs application vector table

Part Number: RM57L843


Hello,

We are building a Bootloader based on the SPNA190 "UART Bootloader for Hercules RM48x MCU'. The goal is to be able to install a software package in the field using the serial interface. The Software Package is a complete stand alone software, with boot, selft-test, kernel and application. The Bootloader reads an input and decides whether to jump to the Software Package or not.

Once the Bootloader will remain in the flash, while the Software Package is running, the arm core vector table (at address 0) will be the Bootloader table. For instance, if a supervisor call (SVC exceptions) occurs, the handler executed will be the Bootloader handler. Am I right? Is there a why to make the MPU to use the Software Package arm core vector table instead?

The Arm Cortex-R Programmer’s Guide says that it is possible to move the vector table to 0xFFFF0000, but this address is reserved for the PMM registers.

I believe there isn't a problem with FIQs and IRQs because they refer to the same VIM table.

Best regards,
Marcio