Part Number: CCSTUDIO-SAFETY
Hi
I want to use the CCS v8.3.1 in project for RM44L520 device instead of the prior CCS v6.1.1.
(Development PC environment is windows-7 32 bit)
And the CCS v8.3.1 includes the ARM-CGT v18.1.4.LTS by default.
But, i would like to use the latest version of ARM-CGT for tool validation of EN50128.
In this case, combinations of the CCS v8.3.1 and ARM-CGT-7-v18.1.8.LTS is compatible?
Or is there a suitable combination for tool verification considering the RM44L520 device and PC environment?