Part Number: MSP432E401Y
Hi
1. I have downloaded the Bootloader code from TI and successfully flashed in msp432e401y Development Board.
2. I also saw in device manager ,its Detected as Stellaries Device Firmware Upgrade
3. so through LM Flash Programmer , i also flashed Application through Stellaries Device Firmware Upgrade using USB Interface
After that, when i was reset the board , bootloader is not calling application.
i ,also share my linker script of both Bootloader and Appllcation .
What changes i need to do so that , bootloader will call application
pls guide me .
Thanks
// Application Linker Script File.
--diag_suppress=10199
--retain=interruptVectors
MEMORY
{
FLASH (RX) : origin = 0x00004000, length = 0x00100000
SRAM (RWX) : origin = 0x20000000, length = 0x00040000
}
/* The following command line options are set as part of the CCS project. */
/* If you are building using the command line, or for some reason want to */
/* define them here, you can uncomment and modify these lines as needed. */
/* If you are using CCS for building, it is probably better to make any such */
/* modifications in your CCS project and leave this file alone. */
/* */
/* --heap_size=0 */
/* --stack_size=256 */
/* --library=rtsv7M4_T_le_eabi.lib */
/* Section allocation in memory */
SECTIONS
{
#ifndef gen_crc_table
.intvecs: > 0x00004000
.text : > FLASH
.const : > FLASH
.cinit : > FLASH
.pinit : > FLASH
.rodata : > FLASH
.init_array : > FLASH
#else
.intvecs: > 0x00004000, crc_table(crc_table_for_intvecs)
.text : > FLASH, crc_table(crc_table_for_text)
.const : > FLASH, crc_table(crc_table_for_const)
.cinit : > FLASH, crc_table(crc_table_for_cinit)
.pinit : > FLASH, crc_table(crc_table_for_pinit)
.rodata : > FLASH, crc_table(crc_table_for_pinit)
.init_array : > FLASH, crc_table(crc_table_for_init_array)
.TI.crctab : > FLASH
#endif
.vtable : > 0x20000000
.data : > SRAM
.bss : > SRAM
.sysmem : > SRAM
.stack : > SRAM
}
__STACK_TOP = __stack + 512;
// Bootloader Linker Script File.
--retain=Vectors
/* The following command line options are set as part of the CCS project. */
/* If you are building using the command line, or for some reason want to */
/* define them here, you can uncomment and modify these lines as needed. */
/* If you are using CCS for building, it is probably better to make any such */
/* modifications in your CCS project and leave this file alone. */
/* */
/* --heap_size=0 */
/* --stack_size=256 */
/* --library=rtsv7M3_T_le_eabi.lib */
/* System memory map */
MEMORY
{
FLASH (RX) : origin = 0x00000000, length = 0x00010000
SRAM (RWX) : origin = 0x20000000, length = 0x00010000
}
/* Section allocation in memory */
SECTIONS
{
GROUP
{
.intvecs
.text
.const
.data
} load = FLASH, run = 0x20000000, LOAD_START(init_load), RUN_START(init_run), SIZE(init_size)
GROUP
{
.bss
.stack
} run = SRAM, RUN_START(bss_run), RUN_END(bss_end), SIZE(bss_size), RUN_END(__STACK_TOP)
}