Part Number: LP-AM243
Other Parts Discussed in Thread: UNIFLASH
Hi expert,
I am using LP-AM243 according to the Getting Started guide's guidance. I power up board by USB Type C first, then connect the Micro USB, there is CCCCCCC printing out in UART booting mode. But I noticed that when I close the UART terminal, it is slightly different from the guidance. Figure 1 is the content displayed when I use it myself, and Figure 2 is the picture displayed in the guidance. My side has no other output behind CCCC. I don't know if this is correct.

Figure 1

Figure 2
And I also encountered a problem that I cannot flash the SOC initialization binary to the LP. I confirmed that there is no problem with my python installation, as shown in Figure 3. But when I enter python uart_uniflash.py -p COM<x> --cfg=sbl_prebuilt/am243x-lp/default_sbl_null.cfg, it will not enter the flashing process, and the error display is shown in Figure 4.

Figure 3

Figure 4
I have checked the "Flash tool error messages and solutions" part of the tutorial but did not find a suitable solution. So could you please kindly help me about this issue? Thanks a lot!
BR
Julia