This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problems with Auto-Initialize on DMA & MIBADC1 RAM



I am having problems getting the DMA and MIBADC1 RAM to auto-init.  The rest of the RAM modules complete successfully.  Even ADC2, so I don't understand why ADC1 does not.   What do I have to do to get the DMA and ADC1 to complete initialization?

I have powered-up all peripherials and enabled them prior to running this code.

 

// enable memory hardware initialization

 

 

p_PSR->u32_MINITGCR = (uint32)0x0000000AU;

 

 

 

 

p_PSR->u32_MSINENA = (uint32)0x0000177F;

 

 

// Wait for memory hardware initialization to complete

 

 

while(((p_PSR->u32_MSTCGSTAT) & (uint32)0x00000100) != (uint32)0x00000100){} ;

 

 

// disable memory hardware initialization

 

 

p_PSR->u32_MINITGCR = (uint32)0x00000005U;

Thanks,

Lacrecia