Part Number: AM2432
Other Parts Discussed in Thread: SYSCONFIG
Hi Team,
My customer has a few questions with regards to using the sysconfig tool.
1. What are the GPMC_CLKLB and MMC1_CLKLB signals? It does not have much relevant documentation in the TRM nor the datasheet and does not seem to connect to any of the pins, but is shown in the tool.
2. When using the sysconfig tool, in the 'Welcome To SysConfig' page, is it the correct procedure to select a 'software product' always? Unless they do not select anything (as below), they cannot see the Power Domains tab (the little icons) on the left-hand side, and the files pinmux_data.c and PinmuxConfigSummary.csv are not generated. Why is it that these files are not generated, and why does the Power Domains tab appear/disappear? Also, how do they know which 'software product' and 'context' to choose?



3. Is the power domain tab not reflected in the code? For example, when using GPMC0_A2(W7) VDDSHV2 and GPMC0_AD4(U18) VDDSHV3 , they set VDDSHV2=1.8V and VDDSHV3=3.3V, but they get a warning.
Best regards,
Mari Tsunoda