Part Number: AM2432
Other Parts Discussed in Thread: SYSCONFIG
Hi Team,
My customer has a questions regarding sysconfig as below.
- We plan to pull RESET_REQz, MCU_RESETz to High, and will not use warm reset. In this situation, when setting the pins, Peripherals->SYSTEM->RESET_REQz and POeripherals->MCU_SYSTEM->MCU_RESETz, do they need to tick these boxes? If they don't and RESET_REQz, MCU_RESETz are open, will these two signals be invalid and will they have issues (such as suddenly resetting)?
- We don't use EMU0, EMU1, MCU_RESETz, RESET_REQz signals, and on PWB these pins are supposed to be un-connected to any node, and we will use internal pull-up resistor on these pins. According to 6.4 Pin Connectivity Requirements on AM243x datasheet, "The internal pull-up may be used to hold a valid logic high level if no PCB signal trace is connected to the ball."
But in Reversed Peripherals->JTAG tab of Sysconfig tool, I can't find the selection of Pullup/Pulldown. Where Can I set the internal pull-up using Sysconfigtool? - In the power domains tab, they set VDDSHV_MCU=3.3V (Other than clock and DDR, all are set to 3.3V). Since MCU domain IO is also 3.3V, they set Peripherals->MCU_SYSTEM->Preferred Voltage to 3.3V. However, they have a voltage conflict with MCU_PORz. As this is most likely due to MCU_PORz is set to VDDSHV_OSC=1.8V (set in domain IO pin). Is it ok to leave this as a conflict.
- Also, is their understanding that MCU_RESETz is set to 3.3V, MCU_PORz is set to 1.8V signals correct?
Best regards,
Mari Tsunoda