This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
My questions here are in reference to datasheet Table 6-85. Connectivity Requirements (ALV Package)
Hello,
1) Yes, E9 and A10 should still be pulled high through external pull resistors even if not using I2C function.
2) These balls are also responsible for setting the device boot mode and therefore must be set to the required valid logic level at boot-time to ensure proper boot mode/sequence.
3) L14 and L15 are the supply pins for VDDSHV5. Even if not using SDIO_LDO, these pins should be connected to the corresponding power supply.
Best Regards,
Zackary Fleenor
Hi Zackary,
For 2) is it OK to permanently connect pull-up/down resistors to balls T20, U21, T18, U20, U19, V20, V21, T17, R16, W20, W21, V18, Y21, Y20 if we are only using to set the desired boot mode? No other devices connected to these pins.
Hello Igor,
Yes, permanent pulls can be implemented via external resistors. SW is in charge of properly setting the associated PADCONFIG registers per application requirements, in this case the default configuration on reset should suffice.
Best Regards,
Zackary Fleenor