This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, I faced with a problem to read data from EEPROM while I bring up F021 library for my project. I initialize FLASH during to recommended state machine description in "F021 FLASH API Version 2.01.01 (page 41)". Here piece of my code:
/************************************************************************************/
uint8_t *flash_addr = F021_EEPROM_MAP_BEGIN; // 0xF0200000U
Fapi_StatusType status;
status = Fapi_isAddressEEPROM(F021_EEPROMECC_MAP_BEGIN);
status = Fapi_initializeFlashBanks(160);
status = Fapi_setActiveFlashBank(7);
status = Fapi_enableEepromBankSectors(1, 0); // write data to sector #0
status = Fapi_issueProgrammingCommand(flash_addr, (uint8_t*)buff, (uint8_t)(8), F021_EEPROMECC_MAP_BEGIN, (uint8_t)(8), Fapi_DataOnly);
//For this functions calls return value is always "Fapi_Status_Success". After that I want to read written by me data from EEPROM to be sure that write operation is correct.
status = Fapi_initializeFlashBanks(160);
status = Fapi_doMarginReadByByte(flash_addr, (uint8_t*)buff, (uint32_t)(8), Fapi_NormalRead);
/************************************************************************************/
But function Fapi_doMarginReadByByte() stalls execution of my program (Some error inside function calls error handler in RTOS). I'm not deep into assembler, but execution crashes in _Fapi_enterMarginMode function in assembler debug.
Also I watch code example from this issue and write the same sequence of calls: https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/1036826/rm48l952-f021-flash-api-usage-examples
Please, help me what's going wrong here.
Hi,
If you use bank 7 as EEPROM to store block of data, you can use TI FEE driver to write data to and read data from the EEPROM . The FEE driver is generated by HALCoGen if FEE is checked, because it was already tested and it is reliable
The TI FEE Driver provides the following functional services:
Initialization:
• TI_Fee_Init
Operations:
• TI_Fee_WriteAsync
• TI_Fee_WriteSync
• TI_Fee_Read
• TI_Fee_ReadSync
• TI_Fee_EraseImmediateBlock
• TI_Fee_InvalidateBlock
• TI_Fee_Shutdown
• TI_Fee_Cancel
• TI_Fee_Format
Information:
• TI_Fee_GetStatus
• TI_Fee_GetJobResult
• TI_Fee_GetVersionInfo
You can refer below user guide
Also HALCoGen providing example project, you can find it in Help window
--
Thanks,
Jagadish.
Hi, I generate a source code from HALCoGen and add it in my project. I use code from FEE read/write example project and also I stalled in TI_Fee_Init() function (Fapi_doBlankCheck in ti_fee_uil.c:903). Init function takes no parameters, so I expected that it not depends from me. As error occurred I think some troubles happens in my code in initialization and etc. May be this functions from FEE library mush run from RAM, in critical code section or some other stuff?
Hi,
It might be due to using of wrong version of the F021_API library.
We should configure "F021_API_CortexR4_LE_L2FMC.lib"
--
Thanks,
Jagadish.