Part Number: TM4C1233H6PM
Hi,
When VDD is 3.3V, and set PD4, PD5 as USB function
Whats the absolute Maximum Ratings of PD4, PD5?
3.3V+0.3 ? or 5.5V?
Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TM4C1233H6PM
Hi,
When VDD is 3.3V, and set PD4, PD5 as USB function
Whats the absolute Maximum Ratings of PD4, PD5?
3.3V+0.3 ? or 5.5V?
Thank you.
Hi,
This is described in the datasheet. Please see below.

10.1 Signal Description
GPIO signals have alternate hardware functions. The following table lists the GPIO pins and their
analog and digital alternate functions. All GPIO signals are 5-V tolerant when configured as inputs
except for PD4, PD5, PB0 and PB1, which are limited to 3.6 V.