Part Number: TMS570LC4357
Other Parts Discussed in Thread: HALCOGEN
Hello,
I am using the TMS570LC4357 and I have a question about the initial configuration value for one of the system registers, General Purpose Register (GPREG1).
In HL_system.c the function systemGetConfigValue() returns either initial or current value for each register.
For the initial value of GPREG1 systemGetConfigValue() returns SYS_GPREG1_CONFIGVALUE.
SYS_GPREG1_CONFIGVALUE is defined in HL_system.c as follows
#define SYS_GPREG1_CONFIGVALUE 0x0005FFFFU
There does not appear to be anywhere within the HALCoGen generated code where GPREG1 is explicitly initialised.
The value of GPREG1 after reset is 0x00000000U - as defined in section 2.5.1.34 General Purpose Register (GPREG1) of the Technical Reference Manual TMS570LC43x 16/32-Bit RISC Flash Microcontroller (SPNU563A March 2018).
Can I therefore assume that the value of SYS_GPREG1_CONFIGVALUE as generated by HALCoGen is wrong and the correct configuration value should be 0x00000000U.
Thank you.