This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
i would like to ask if the table bellow is correct or not - checking technical reference manual spnu563.pdf of TMS570LC4357 processor,
because the VCLK3 is clocked at 75 MHz at TMS570LC4357, so it confuses me because the calculation does not correspond to this timing.
Can u please correct me or tell me what is right?
BR
JZ
Hi JZ,
The values are corresponds to the frequency of 60Mhz
And the values are rounded by 2 decimals like as highlighted in above excel formula.
But yes they didn't mentioned this frequency at the table, so it is confusing. I will take necessary action to correct our TRM and many thanks for pointing out this typo.
--
Thanks & Regards,
Jagadish.
Okay, thanks for explanation. Yes, i could be fine to insert this information into TRM.
BR
JZ