Hi QJ Wang
Is it possible to flash the Bootloader SW in any other location instead of 0x00000000.
If it is possible how to set the flash start address for bootloader using HL_sys_link.cmd ?
| Software (BOOT or APPL) | Sub- Division Memory | Sub- Division Memory Range | Memory length (HEX) |
| BOOT | VECTORS | 0x00000000 - 0x00000020 | 0x00000020 |
| FLASH0 | 0x00000020 - 0x000FFFFF | 0x000FFFDF | |
| APPL | APP_STATUS_ADDRESS | 0x00100000 - 0x00100020 | 0x00000020 |
| VECTORS | 0x00100020 - 0x00100040 | 0x00000020 | |
| FLASH1 | 0x00100040 - 0x003FFFFF | 0x002FFFBF |
Thanks in advance.
Santhosh.