Part Number: TMS570LC4357
Other Parts Discussed in Thread: TMS570LS3137
Hello,
We have a customer who has a custom development board using the TMS570LS3137 ARM chip. They prefer the Lauterbach debugger T32 with a LA-3253 debug cable. This setup works and we can program and debug with it. Now we want to switch to CCS + XDS200 debugger and it doesn't work with the provided "20e_cTI-20t_ARM Pin Converter" connector.
The connectors should be the same 20 pin ARM and I don't see any reason why it shouldn't work out of the box?
Can you support me with this issue?


[Start: Texas Instruments XDS2xx USB Debug Probe]
Execute the command:
%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -S integrity
[Result]
-----[Print the board config pathname(s)]------------------------------------
C:\Users\D4854~1.SAJ\AppData\Local\TEXASI~1\
CCS\ccs1200\0\0\BrdDat\testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 560/2xx-class product.
This utility will load the program 'xds2xxu.out'.
The library build date was 'Jun 18 2022'.
The library build time was '03:06:08'.
The library package version is '9.8.0.00235'.
The library component version is '35.35.0.0'.
The controller does not use a programmable FPGA.
The controller has a version number of '13' (0x0000000d).
The controller has an insertion length of '0' (0x00000000).
This utility will attempt to reset the controller.
This utility has successfully reset the controller.
-----[Print the reset-command hardware log-file]-----------------------------
This emulator does not create a reset log-file.
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-233' (0xffffff17).
The title is 'SC_ERR_PATH_BROKEN'.
The explanation is:
The JTAG IR and DR scan-paths cannot circulate bits, they may be broken.
An attempt to scan the JTAG scan-path has failed.
The target's JTAG scan-path appears to be broken
with a stuck-at-ones or stuck-at-zero fault.
[End: Texas Instruments XDS2xx USB Debug Probe]