Part Number: TMDS243GPEVM
Other Parts Discussed in Thread: UNIFLASH
Our customer sees OSPI boot fail on TMDS243GPEVM.
In the following procedure, after successful flashing by UART boot, nothing is output on the UART terminal by OSPI boot.
software-dl.ti.com/.../EVM_SETUP_PAGE.html
When using other boards (TMDS243GPEVM or TMDS64GPEVM), our customer can see the output on the UART terminal by the same procedure.
On any board, the BOOTMODE value in both the CTRLMMR_MAIN_DEVSTAT register (4300 0030h) and the CTRLMMR_MAIN_BOOTCFG register (4300 0034h) shows "0000 0273h".
Incidentally, SOC Initialization using CCS Scripting can be successfully performed in the following procedure.
software-dl.ti.com/.../EVM_SETUP_PAGE.html
If the EVM is broken, our customer wants to replace it with a new one.
Best regards,
Daisuke