Part Number: TMS570LC4357
Other Parts Discussed in Thread: HALCOGEN
hi iam using TMS570LC43X evalution board(MASTER) i want to communicate with (SLAVE)arinc holt board(hi-3593) using spi(SPI3) iam not able to read the date from slave pls help me out any refrence example wil be good iam beginer in tms570.
void spiInit(void)
{
/* USER CODE BEGIN (2) */
/* USER CODE END */
/** @b initialize @b SPI3 */
/** bring SPI out of reset */
spiREG3->GCR0 = 0U;
spiREG3->GCR0 = 1U;
/** SPI3 master mode and clock configuration */
spiREG3->GCR1 = (spiREG3->GCR1 & 0xFFFFFFFCU) | ((uint32)((uint32)1U << 1U) /* CLOKMOD */
| 1U); /* MASTER */
/** SPI3 enable pin configuration */
spiREG3->INT0 = (spiREG3->INT0 & 0xFEFFFFFFU) | (uint32)((uint32)0U << 24U); /* ENABLE HIGHZ */
/** - Delays */
spiREG3->DELAY = (uint32)((uint32)255U << 24U) /* C2TDELAY */
| (uint32)((uint32)255U << 16U) /* T2CDELAY */
| (uint32)((uint32)0U << 8U) /* T2EDELAY */
| (uint32)((uint32)0U << 0U); /* C2EDELAY */
/** - Data Format 0 */
spiREG3->FMT0 = (uint32)((uint32)0U << 24U) /* wdelay */
| (uint32)((uint32)0U << 23U) /* parity Polarity */
| (uint32)((uint32)0U << 22U) /* parity enable */
| (uint32)((uint32)0U << 21U) /* wait on enable */
| (uint32)((uint32)0U << 20U) /* shift direction */
| (uint32)((uint32)0U << 17U) /* clock polarity */
| (uint32)((uint32)0U << 16U) /* clock phase */
| (uint32)((uint32)74U << 8U) /* baudrate prescale */
| (uint32)((uint32)8U << 0U); /* data word length */
/** - Data Format 1 */
spiREG3->FMT1 = (uint32)((uint32)0U << 24U) /* wdelay */
| (uint32)((uint32)0U << 23U) /* parity Polarity */
| (uint32)((uint32)0U << 22U) /* parity enable */
| (uint32)((uint32)0U << 21U) /* wait on enable */
| (uint32)((uint32)0U << 20U) /* shift direction */
| (uint32)((uint32)0U << 17U) /* clock polarity */
| (uint32)((uint32)0U << 16U) /* clock phase */
| (uint32)((uint32)74U << 8U) /* baudrate prescale */
| (uint32)((uint32)16U << 0U); /* data word length */
/** - Data Format 2 */
spiREG3->FMT2 = (uint32)((uint32)0U << 24U) /* wdelay */
| (uint32)((uint32)0U << 23U) /* parity Polarity */
| (uint32)((uint32)0U << 22U) /* parity enable */
| (uint32)((uint32)0U << 21U) /* wait on enable */
| (uint32)((uint32)0U << 20U) /* shift direction */
| (uint32)((uint32)0U << 17U) /* clock polarity */
| (uint32)((uint32)0U << 16U) /* clock phase */
| (uint32)((uint32)74U << 8U) /* baudrate prescale */
| (uint32)((uint32)16U << 0U); /* data word length */
/** - Data Format 3 */
spiREG3->FMT3 = (uint32)((uint32)0U << 24U) /* wdelay */
| (uint32)((uint32)0U << 23U) /* parity Polarity */
| (uint32)((uint32)0U << 22U) /* parity enable */
| (uint32)((uint32)0U << 21U) /* wait on enable */
| (uint32)((uint32)0U << 20U) /* shift direction */
| (uint32)((uint32)0U << 17U) /* clock polarity */
| (uint32)((uint32)0U << 16U) /* clock phase */
| (uint32)((uint32)74U << 8U) /* baudrate prescale */
| (uint32)((uint32)16U << 0U); /* data word length */
/** - set interrupt levels */
spiREG3->LVL = (uint32)((uint32)0U << 9U) /* TXINT */
| (uint32)((uint32)0U << 8U) /* RXINT */
| (uint32)((uint32)0U << 6U) /* OVRNINT */
| (uint32)((uint32)0U << 4U) /* BITERR */
| (uint32)((uint32)0U << 3U) /* DESYNC */
| (uint32)((uint32)0U << 2U) /* PARERR */
| (uint32)((uint32)0U << 1U) /* TIMEOUT */
| (uint32)((uint32)0U << 0U); /* DLENERR */
/** - clear any pending interrupts */
spiREG3->FLG |= 0xFFFFU;
/** - enable interrupts */
spiREG3->INT0 = (spiREG3->INT0 & 0xFFFF0000U)
| (uint32)((uint32)0U << 9U) /* TXINT */
| (uint32)((uint32)0U << 8U) /* RXINT */
| (uint32)((uint32)0U << 6U) /* OVRNINT */
| (uint32)((uint32)0U << 4U) /* BITERR */
| (uint32)((uint32)0U << 3U) /* DESYNC */
| (uint32)((uint32)0U << 2U) /* PARERR */
| (uint32)((uint32)0U << 1U) /* TIMEOUT */
| (uint32)((uint32)0U << 0U); /* DLENERR */
/** @b initialize @b SPI3 @b Port */
/** - SPI3 Port output values */
spiREG3->PC3 = (uint32)((uint32)1U << 0U) /* SCS[0] */
| (uint32)((uint32)1U << 1U) /* SCS[1] */
| (uint32)((uint32)1U << 2U) /* SCS[2] */
| (uint32)((uint32)1U << 3U) /* SCS[3] */
| (uint32)((uint32)1U << 4U) /* SCS[4] */
| (uint32)((uint32)1U << 5U) /* SCS[5] */
| (uint32)((uint32)0U << 8U) /* ENA */
| (uint32)((uint32)0U << 9U) /* CLK */
| (uint32)((uint32)0U << 10U) /* SIMO */
| (uint32)((uint32)0U << 11U); /* SOMI */
/** - SPI3 Port direction */
spiREG3->PC1 = (uint32)((uint32)1U << 0U) /* SCS[0] */
| (uint32)((uint32)1U << 1U) /* SCS[1] */
| (uint32)((uint32)1U << 2U) /* SCS[2] */
| (uint32)((uint32)1U << 3U) /* SCS[3] */
| (uint32)((uint32)1U << 4U) /* SCS[4] */
| (uint32)((uint32)1U << 5U) /* SCS[5] */
| (uint32)((uint32)0U << 8U) /* ENA */
| (uint32)((uint32)1U << 9U) /* CLK */
| (uint32)((uint32)1U << 10U) /* SIMO */
| (uint32)((uint32)0U << 11U); /* SOMI */
/** - SPI3 Port open drain enable */
spiREG3->PC6 = (uint32)((uint32)0U << 0U) /* SCS[0] */
| (uint32)((uint32)0U << 1U) /* SCS[1] */
| (uint32)((uint32)0U << 2U) /* SCS[2] */
| (uint32)((uint32)0U << 3U) /* SCS[3] */
| (uint32)((uint32)0U << 4U) /* SCS[4] */
| (uint32)((uint32)0U << 5U) /* SCS[5] */
| (uint32)((uint32)0U << 8U) /* ENA */
| (uint32)((uint32)0U << 9U) /* CLK */
| (uint32)((uint32)0U << 10U) /* SIMO */
| (uint32)((uint32)0U << 11U); /* SOMI */
/** - SPI3 Port pullup / pulldown selection */
spiREG3->PC8 = (uint32)((uint32)1U << 0U) /* SCS[0] */
| (uint32)((uint32)1U << 1U) /* SCS[1] */
| (uint32)((uint32)1U << 2U) /* SCS[2] */
| (uint32)((uint32)1U << 3U) /* SCS[3] */
| (uint32)((uint32)1U << 4U) /* SCS[4] */
| (uint32)((uint32)1U << 5U) /* SCS[5] */
| (uint32)((uint32)1U << 8U) /* ENA */
| (uint32)((uint32)1U << 9U) /* CLK */
| (uint32)((uint32)1U << 10U) /* SIMO */
| (uint32)((uint32)1U << 11U); /* SOMI */
/** - SPI3 Port pullup / pulldown enable*/
spiREG3->PC7 = (uint32)((uint32)0U << 0U) /* SCS[0] */
| (uint32)((uint32)0U << 1U) /* SCS[1] */
| (uint32)((uint32)0U << 2U) /* SCS[2] */
| (uint32)((uint32)0U << 3U) /* SCS[3] */
| (uint32)((uint32)0U << 4U) /* SCS[4] */
| (uint32)((uint32)0U << 5U) /* SCS[5] */
| (uint32)((uint32)0U << 8U) /* ENA */
| (uint32)((uint32)0U << 9U) /* CLK */
| (uint32)((uint32)0U << 10U) /* SIMO */
| (uint32)((uint32)0U << 11U); /* SOMI */
/* SPI3 set all pins to functional */
spiREG3->PC0 = (uint32)((uint32)1U << 0U) /* SCS[0] */
| (uint32)((uint32)1U << 1U) /* SCS[1] */
| (uint32)((uint32)1U << 2U) /* SCS[2] */
| (uint32)((uint32)1U << 3U) /* SCS[3] */
| (uint32)((uint32)1U << 4U) /* SCS[4] */
| (uint32)((uint32)1U << 5U) /* SCS[5] */
| (uint32)((uint32)0U << 8U) /* ENA */
| (uint32)((uint32)1U << 9U) /* CLK */
| (uint32)((uint32)1U << 10U) /* SIMO */
| (uint32)((uint32)1U << 11U); /* SOMI */
/** - Initialize TX and RX data buffer Status */
g_spiPacket_t[2U].tx_data_status = SPI_READY;
g_spiPacket_t[2U].rx_data_status = SPI_READY;
/** - Finally start SPI3 */
spiREG3->GCR1 = (spiREG3->GCR1 & 0xFEFFFFFFU) | 0x01000000U;
/* USER CODE BEGIN (3) */
/* USER CODE END */
}
/*************************************************************MAIN PROGRAM***********************************************/
U16 TX_Data_Master[8] = {0X04, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00};
U16 TX_Data_Master1[8] = {0x08, 0x03, 0x00, 0x70, 0x00, 0x00, 0x00, 0x00};
U16 TX_Data_Master2[8] = {0x80, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00};
U16 RX_Data_Master[8] = {0};
spiDAT1_t dataconfig1_t;
dataconfig1_t.CS_HOLD = TRUE;
dataconfig1_t.WDEL = FALSE;
dataconfig1_t.DFSEL = SPI_FMT_0;
dataconfig1_t.CSNR = 0xFB;
spiInit();
//Reset holt
// spiTransmitData(spiREG1, &dataconfig1_t, 1, TX_Data_Master );
//[TCR] <= 0X03
spiTransmitData(spiREG3, &dataconfig1_t, 2, TX_Data_Master1);
spiTransmitAndReceiveData(spiREG3, &dataconfig1_t, 2, TX_Data_Master2, RX_Data_Master);
}