Part Number: AM2434
Other Parts Discussed in Thread: SYSCONFIG
Hi expert,
When I used SDK(8.4.0.17) demo code on AM243x Launch Pad, R5fss0_0 - GPIO IRQ module only has Router8 & Router9, but reference TRM R5fss0_0 - GPIO IRQ module should be set from Router0 to Router15

I referenced the forums :. [FAQ] AM6442: How to configure the GPIO interrupt - Processors forum - Processors - TI E2E support forums
In AM243x SDK file " sciclient_defaultBoardcfg_rm.c " also set .num_resource = 2 & .start_resource = 8 to limit R5fss0_0 - GPIO IRQ module

Can I change two paramters that is equal to .num_resource = 16 & .start_resource = 0, let R5fss0_0 - GPIO IRQ module to use all GPIO mux ?
If I can, please tell me the modify method.
I already tried to modify the source code & use makefile rebuild the all library of the SDK, but I can't get the correct result.
So. please tell me the correct method to modify the Router setting.
Regards
Bolt