This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2434: How to configure GPIO MUX INTRTR0 router

Part Number: AM2434
Other Parts Discussed in Thread: SYSCONFIG

Hi expert,

     When I used SDK(8.4.0.17) demo code on AM243x Launch Pad, R5fss0_0 - GPIO IRQ module only has Router8 & Router9, but reference TRM R5fss0_0 - GPIO IRQ module should be set  from Router0 to Router15 

         

      I referenced the forums :. [FAQ] AM6442: How to configure the GPIO interrupt - Processors forum - Processors - TI E2E support forums

     In AM243x SDK file  " sciclient_defaultBoardcfg_rm.c " also set .num_resource = 2  & .start_resource = 8 to limit R5fss0_0 - GPIO IRQ module

            

          Can I change two paramters that is equal to .num_resource = 16  & .start_resource = 0, let R5fss0_0 - GPIO IRQ module to use all GPIO mux ?

          If I can, please tell me the modify method.

          I already tried to modify the source code & use makefile rebuild the all library of the SDK, but I can't get the correct result.

          So. please tell me the correct method to modify the Router setting.

Regards

Bolt