Part Number: AM2434
Other Parts Discussed in Thread: AM2432, DP83869
Tool/software:
Hi team,
I'm currently working with AM2432 + DP83822 PHY for Industrial communication
This custom board was designed by taking AM243 LP as reference.
In LP, MUX IC was connected between SoC and DP83869 in PHY 1 side for selection between CPSW and PRG lines.
MUX_SEL pin is configured pulled high and low based on the requirement.

As per requirement, we have removed the MUX IC and have taken PRG1_RGMII1 lines connected directly from SoC to PHY 1

EtherCAT Slave simple demo code uses PRG1 lines for communication(MUX SEL was not configured and it was pulled low by default) and currently we are using same for testing with DP83822 driver.
PHY 2 is connected with PC(TwinCAT - EtherCAT protocol) and working fine.
I'm having Issues connecting PC(TwinCAT - EtherCAT protocol) with PHY1.
I tried different configuration for custom board and got PHY2 working after the below configurations

Is MUX removal a issue? Do I need to configure anything in software for MUX removal in EtherCAT slave simple demo code?
Regards,
D. Jenita