Part Number: TM4C1294NCPDT
Hi
Are the RO type registers Read Only?
I wrote Register 92: Ethernet PHY BIST Control - MR22 (EPHYBISTCR) @bit6 to 1.

(I think this register is RO.)
But softwere can write the register 1.

(MR22_BISTCR is user defined int value)

This picture shows UART output.
0x100 : before write MR22 (EPHYBISTCR) @bit6.(shows reset value)
0x140 : after write MR22 (EPHYBISTCR) @bit6 to1.
thanks,
GR