This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Customer is setting EtherNet/IP Conformance Test tool and using AM243-LP as DUT(Device Under Test) to run test.
In order to reproduce the test environment, They have some questions about setting.
Do they need to check the below checkbox?
Hi AndreTseng,
Do they need to check the below checkbox?
- Type 1 or 2 Reset
- Profile Verification
- Encapsulation
Yes, These are compulsory test as per ODVA and we test our DUT for above three.
BR
Customer report they have problem after they turn on Profile Verification and Encapsulation. They are using SDK 8.4.
Can you please provide some suggestions to pass tests?
Regards
Andre
CT19_am243x-lp_tiEtherNetIP_freeRTOS_Identity_ProfileVerificationTest_Encapsolation_Selection.log
Hi Andre,
Customer report they have problem after they turn on Profile Verification and Encapsulation. They are using SDK 8.4.
TI highly recommends using latest SDK version, as this comes with bug fixes which are reported on previous SDK.
I will check regarding the conformance test results on SDK 8.04. Let me get info from internal team on this. I will try to get back by early next week. Thanks
Nilabh
Customer report they have the same issue when they use SDK 8.5. Can you please check or provide our own test log?
Regards
Andre
Nilabh,
Customer has used the version 8.5 to re-test all cases below with the .soc file setting from the SDK, and update the test issues below:
They got 6 errors and 3 warning from the conformance test.
The error below happens when running the “Profile Verification” test.
1> *** EtherNet/IP Devices undergoing certification for the first time and multi-port devices receiving an update that adds CIP functionality are required to implement LLDP protocol and LLDP Management Object starting from May 2022.
Another 2 errors happen when running the “Time Sync” test in line 1217 and line 1234.
1217 1> *** This attribute is required if 1. A device supports more than one CIP port and it's impossible for the PTP port and CIP port numbers to be the same; or 2. More than one PTP port is associated with a single CIP port (e.g. PRP). Otherwise the error can be waived.
When they did the “DLR” and “QoS” tests, they also receive another error at line 1781.
1781 1> *** Didn't receive valid Learning_Update Frame from DUT within 100 milliseconds.
The “TCP/IP” and the “Ethernet Link” tests shows another error as below.
3357 1> *** Attribute data value incorrect attr 3, Srv Code x0E
There is 1 warning they received from the “Identity” test.
434 1> ** Warning: It is highly recommended to support Identity Object Class Revision 2.
Another 2 warning they received from the “Assembly” test.
2041 1> ** Warning: No data in the Data attribute. Please verify if it's acceptable.2572 1> ** Warning: No data in the Data attribute. Please verify if it's acceptable.
The log files are as attachments.
They would like to know if these issues are caused by known firmware issues or by test configurations?
How to fix these problems?
Regards
AndreAssembly+ConnectionMessage.logDLR+QoS.logIdentity.logMessageRouter.logTCPIP+EtherNetLink.logTimeSync.log
Hi Andres,
are we sure that they have configured their host PC (on which the test runs) and the IP addresses in the test tool itself correctly?
On the host PC one is required to configure 2 consecutive IP addresses on the network port that is connected to the target, for example 192.168.1.1/24 and 192.168.1.2/24. Also on the Run Test tab page, there are the Select DUP IP Addresses and Select Host IP Addresses pull-down menus that are frequently wrong when one starts CT19. They need to make also sure that MAC addresses are correct.
The LLDP error message is known, but addressed with later revisions of the stack (the did not made it into the SDK yet due to problems with the SDK RC for 8.4 and 8.5)
Regards
Nilabh
Nilabh,
After customer corrects the MAC setting, the error in DLR test is fixed, but other 3 test issues are remained. They also confirm all NIC configuration follow the descriptions in CT19 help manual.
Can you please help for the following problems in “Time Sync” and “Ethernet Link” tests?
Time Sync test:
2 errors happen when running the “Time Sync” test in line 1217 and line 1234.
1217 1> *** This attribute is required if 1. A device supports more than one CIP port and it's impossible for the PTP port and CIP port numbers to be the same; or 2. More than one PTP port is associated with a single CIP port (e.g. PRP). Otherwise the error can be waived.
The “Ethernet Link” tests shows another error as below.
3357 1> *** Attribute data value incorrect attr 3, Srv Code x0E
Additionally, to those warning messages they need TI’s answers if it will be fixed or not.
There is 1 warning I received from the “Identity” test.
434 1> ** Warning: It is highly recommended to support Identity Object Class Revision 2.
Another 2 warning I received from the “Assembly” test.
2041 1> ** Warning: No data in the Data attribute. Please verify if it's acceptable.2572 1> ** Warning: No data in the Data attribute. Please verify if it's acceptable.
They also suddenly get a “License Expired” message from the UART port. It seems causing lots of errors when doing the encapsulation test and never happened before.
Could you help customer to figure out what’s going on and how to fix it?
Thank you for your help.
Regards
Andre
Hi Andrea,
Can you please help for the following problems in “Time Sync” and “Ethernet Link” tests?
Let me check on the error with the team internally.
hey also suddenly get a “License Expired” message from the UART port. It seems causing lots of errors when doing the encapsulation test and never happened before.
Could you help customer to figure out what’s going on and how to fix it?
For this could you please tell me if you are using F variant of AM243 or not?
Nilabh,
They are using XAM2434BSFGGIALX(HS-FS) device. Any issue with this sample?
Regards
Andre
Hi Andreas,
They are using XAM2434BSFGGIALX(HS-FS) device. Any issue with this sample?
F samples should not have given this issue. Let me check this internally.
Can you please help for the following problems in “Time Sync” and “Ethernet Link” tests?
Concerning the Time Sync test, this error message can be ignore, i.e. 'waived' as ODVA calls it. This was confirmed to us by ODVA. as we have only one PTP port that is used by both Ethernet Link instances
Concerning the Ethernet Link test error, we strongly assume that the physical MAC address is not configured correctly. It has to be set both in 246 Ethernet Link - Instance Group 1 and under Physical Data - TCP Interface 1.
Concerning the Warning on the Identity Object, this is work in progress, as we need this to support Vol 7C IO-Link gateways.
Finally, the Assembly test warning, this can be ignored.
Nilabh,
More questions from customer, they still have problems when they test QoS by ODVA conformance tool to CT19.1.
ACD full test report.xmlACD full test report.html
All failing tests are relevant to two issues of “the response behavior when a conflict is detected” and “ACD timing verifying”. The screen clips are as attachments of the two .PNG files.
Do you know what may cause these behaviors fail?
Regards
Andre
Hi Andrea,
we are looking into the issues, let me get back on it once I have an update
Hi Andrea,
the issues in the ACT test reported above we cannot reproduce here. We see one ACD issue here reported by the CT19.1 scripts, but this is not one of those above. This is currently investigated.
Concerning the messages above, do you happen to have a Wireshark trace, as from the HTML file we don't get enough detail.
The ACD test seems to be tricky once in a while (from the user perspective) thus a Wireshark trace may help to identify the real issue for the messages above. As mentioned, with our current software status we don't see those messages and nothing had been changed related to ACD since the 8.4 release.
Can you please help with the wireshark trace here.
Customer re-tested the ACD fail test cases 3.7, 3.8, and collected the Wireshark data.
Please see the attachments. The Wireshark data is between the PC and the Hub A, according the ACD hardware setup from ODVA.
<html xmlns:xsi="http://www.w3.org/2001/XMLSchema-instance" xmlns:xs="http://www.w3.org/2001/XMLSchema-datatypes"> <head> <META http-equiv="Content-Type" content="text/html; charset=utf-8"> <style> table { border-collapse: collapse; width: 100%; } table, th, td { border: 1px solid black; } th, td { text-align: left; padding: 8px; } th { background-color: #4CAF50; color: white; } tr:nth-child(even){background-color: #f2f2f2} </style> </head> <body> <h1>EtherNet/IP ODVA Conformance Test Results</h1> <h2> Test: ACD Behavior Test (Skip LED test)<br> Version: 2.4.13<br> TimeStamp: 2023-04-28T17:10:26.1378059+08:00<br> Elapsed Seconds: 361.4328665<br> Test Engineer: hiwin<br> Authentication: AuthenticationInvalid<br> Test Result: FAIL<dl> <dt>Testware:</dt> <dd>EtherNet/IP CT19-EN Single User License. Licensed to Su, Bo-Cheng, HIWIN MIKROSYSTEM CORP..<br></dd> </dl> </h2> <table> <tr> <th>Test Step</th> <th>Description</th> <th>Result</th> </tr> <tr> <td>InitializeRoutine</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|―0.1 - Enter Test Engineer Info</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|―0.2 - SelectIpAddress</td> <td>Ethernet 4: 192.168.1.4</td> <td>PASS</td> </tr> <tr> <td>|―0.2.1 - Configure Adapter</td> <td>Network adapter 'Intel(R) Ethernet Server Adapter I350-T2' on local host:192.168.1.4</td> <td>PASS</td> </tr> <tr> <td>|―0.3 - Load STC File</td> <td>E2_A1_am243x-lp_tiEtherNetIP_freeRTOS_hiwin</td> <td>PASS</td> </tr> <tr> <td>|―0.3.1 - Initialize Script With STC Values</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――SUB5 - Initialize Script With STC Values</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――S5.1 Assign DUT IP Address</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――S5.1.0 - DUT IP Address</td> <td bgcolor="#cccccc">192.168.1.10</td> <td bgcolor="#cccccc">Test Note</td> </tr> <tr> <td>|――――S5.2 Assign DUT MAC Address</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――S5.3 Assign Reset Timer</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――S5.4 Generate pcap Filter for Arp from DUT only with IP</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――S5.5 Generate pcap Filter for ARP or use of IP address from DUT</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――S5.6 Generate pcap Filter for ARP probe/announce only</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――S5.7 Generate pcap Filter for gratuitous ARP</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――S5.8 Assign PC Address as gateway</td> <td>192.168.1.4</td> <td>PASS</td> </tr> <tr> <td>|――――S5.9 Generate pcap Filter for ARP from DUT with conflict address</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――S5.10 Assign Message Wait Time</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|―0.3.5 - Verify Test Setup</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|―0.4 - List Identity</td> <td></td> <td>N/A</td> </tr> <tr> <td>|――192.168.1.10</td> <td>EtherNet/IP(tm) ADPT am243x-lp</td> <td></td> </tr> <tr> <td>|―0.4.1 - Did ListIdentity fail?</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|―0.5 - Register Session</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――SUB3 - Register Session</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――S3.1 Register Session Try Loop</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――――S3.1 Register Session Try Loop[1]</td> <td bgcolor="lightgray"> </td> <td bgcolor="lightgray">SKIP</td> </tr> <tr> <td>|――――――――S3.1.1 RegisterSession</td> <td></td> <td>N/A</td> </tr> <tr> <td>|――――――――S3.1.2 Break out of loop if RegisterSession succeeded</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――――――――BreakStep</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――S3.2 Check for failed RegisterSession</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|―0.5 - Verify DUT is alive</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|―0.6 - Determine TCPIP Instance number</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――SUB16 - Find Associated TCP/IP Interface Instance</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――S16.0.1 - Get Max Number of TCPIP Instances</td> <td> Status 0x 0014</td> <td>N/A</td> </tr> <tr> <td>|――――S16.0.2 - If Success Record number</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――S16.1 - Loop Through TCPIP Instances</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――――S16.1 - Loop Through TCPIP Instances[1]</td> <td bgcolor="lightgray"> </td> <td bgcolor="lightgray">SKIP</td> </tr> <tr> <td>|――――――――S16.1.1 - Set Instance to Iteration Number</td> <td>1</td> <td>PASS</td> </tr> <tr> <td>|――――――――S16.1.2 - Get Interface Configuration Attribute</td> <td>0A01A8C000FFFFFF0101A8C000000000000000000000</td> <td>N/A</td> </tr> <tr> <td>|――――――――S16.1.3 - If Get Attribute is successful, Check its value</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――――――――S16.1.3 - Get IP Address</td> <td>192.168.1.10</td> <td>PASS</td> </tr> <tr> <td>|――――――――――S16.1.4 - Does this TCPIP Instance Match?</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――――――――――S16.1.5 - Active TCPIP Instance Number</td> <td>1</td> <td>PASS</td> </tr> <tr> <td>|――――――――――――S16.1.6 - Break loop</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――Record the TCP/IP Object Interface being used</td> <td bgcolor="#cccccc">1</td> <td bgcolor="#cccccc">Test Note</td> </tr> <tr> <td>|―0.7 - Determine IP Configuration Method</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――SUB18 - Determine IP Configuration Method</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――S18.1 - Get TCP/IP Attribute 3</td> <td>00000000</td> <td>PASS</td> </tr> <tr> <td>|――――S18.2 - Get Configuration Method bits 0-3</td> <td><hex>00</hex></td> <td>PASS</td> </tr> <tr> <td>|――――S18.3 - Is this static address?</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――――S18.3a - Static Address</td> <td bgcolor="#cccccc">S18: DUT IP Configuration Method: STATIC VALUES</td> <td bgcolor="#cccccc">Test Note</td> </tr> <tr> <td>|――――――S18.3a.2 - Disable DHCP Steps</td> <td>Bypass</td> <td>PASS</td> </tr> <tr> <td>|――――S18.3 - Else</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|―0.8 - Ensure DHCP Server is not running</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|―0.9 Ensure Second port not connected</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――SUB26 - Disconnect Second Port</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――S26.1 - Is External Disconnect 2 Available?</td> <td> </td> <td>PASS</td> </tr> <tr> <td bgcolor="red">MainRoutine</td> <td> </td> <td bgcolor="red">FAIL</td> </tr> <tr> <td>|―1.0 Verify Default Values</td> <td bgcolor="lightgray">*** SKIPPED ***</td> <td bgcolor="lightgray">SKIP</td> </tr> <tr> <td>|―2.0 Attribute 10 Behavior Test</td> <td bgcolor="lightgray">*** SKIPPED ***</td> <td bgcolor="lightgray">SKIP</td> </tr> <tr> <td>|―3.1 & 3.2 Attribute 11 Conflict Record Verification - ACD Activity 02 or 03</td> <td bgcolor="lightgray">*** SKIPPED ***</td> <td bgcolor="lightgray">SKIP</td> </tr> <tr> <td>|―3.3 Attribute 11 set test</td> <td bgcolor="lightgray">*** SKIPPED ***</td> <td bgcolor="lightgray">SKIP</td> </tr> <tr> <td>|―3.4 & 3.5 Attribute 11 Conflict Record Verification - ACD Activity 01</td> <td bgcolor="lightgray">*** SKIPPED ***</td> <td bgcolor="lightgray">SKIP</td> </tr> <tr> <td>|―3.6 Attribute 11 reset via Type 1 Reset service to the Identity object</td> <td bgcolor="lightgray">*** SKIPPED ***</td> <td bgcolor="lightgray">SKIP</td> </tr> <tr> <td bgcolor="red">|―3.7 & 3.8 Attribute 11 Conflict Record Verification - ACD Activity 01</td> <td> </td> <td bgcolor="red">FAIL</td> </tr> <tr> <td bgcolor="red">|―――3.7 Attribute 11 conflict record verification - ACD Activity 01 (ARP announce conflict)</td> <td> </td> <td bgcolor="red">FAIL</td> </tr> <tr> <td>|―――――3.7.0 Embed PCAP Message</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――――SUB17 - Insert Message into PCAP Trace</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――――――S17.0 OpenAdapter</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――――――――S17.1 Embed message into PCAP Trace</td> <td>3.7 ACD Activity 01 </td> <td>PASS</td> </tr> <tr> <td>|―――――Power Cycle</td> <td> </td> <td>N/A</td> </tr> <tr> <td>|――――――SUB4 - Cycle Power</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――――――S4.1 Ensure session is unregistered</td> <td></td> <td>N/A</td> </tr> <tr> <td>|――――――――S4.2 Power Off Command - External</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――――――S4.3 Power Off - Internal</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――――――――S4.3 Power Off</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――――――S4.4 Turn on DHCP Server, if needed</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|―――――――――SUB19 - Start DHCP Server</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――――――S4.5 Settling Time - External</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――――――S4.6 Settling Time - Internal</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――――――――S4.6.1 Power Off Settling Time</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――――――S4.7 Power On Command - External</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――――――S4.8 - Power On Internal</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――――――――S4.9 Power On</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|―――――3.7 OpenAdapter</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|―――――――3.7.1 Start Acquisition</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|―――――――3.7.2 Wait for Initial Probe</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|―――――――3.7.3 Send a conflicting ARP announce</td> <td><hex>000108000604000100216C123456C0A8010A000000000000C0A8010A</hex></td> <td>PASS</td> </tr> <tr> <td>|―――――――3.7.3.1 Stop DHCP Server</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――――――SUB20 - Stop DHCP Server</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|―――――――3.7.4 CompleteAcquisition</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|―――――3.7.5 Verify LED Operation</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――――SUB22 - Verify LED Operation</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|―――――3.7.6 Verify DUT doesn't respond</td> <td> </td> <td>N/A</td> </tr> <tr> <td>|――――――SUB21 - Short RegisterSession</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――――――S21 - RegisterSession Test</td> <td></td> <td>N/A</td> </tr> <tr> <td bgcolor="red">|―――――3.7.7 Verify DUT doesn't respond after a conflict is detected.</td> <td> </td> <td bgcolor="red">FAIL</td> </tr> <tr> <td>|―――――――UnregisterSession</td> <td></td> <td>PASS</td> </tr> <tr> <td bgcolor="red">|―――――――3.7.7 DUT must not respond after a conflict is detected</td> <td bgcolor="yellow">3.7.4 DUT must not respond after a conflict is detected.</td> <td bgcolor="red">FAIL</td> </tr> <tr> <td bgcolor="red">|―――3.8 Attribute 1 and 11 conflict record verification - ACD Activity 01</td> <td> </td> <td bgcolor="red">FAIL</td> </tr> <tr> <td>|―――――3.8.0 Embed PCAP Message</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――――SUB17 - Insert Message into PCAP Trace</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――――――S17.0 OpenAdapter</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――――――――S17.1 Embed message into PCAP Trace</td> <td>3.8 Attribute 1 & 11 Conflict Record Verification</td> <td>PASS</td> </tr> <tr> <td>|―――――3.8.1 Verify AcdStatus Bit</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――――SUB7 - Verify AcdStatus Bit after conflict</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――――――S7.0 Enable DHCP support if needed</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|―――――――――SUB19 - Start DHCP Server</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――――――S7.1 Disconnect Media</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|―――――――――SUB24 - Disconnect Media</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|―――――――――――S24.1 - Is External Media Disconnect Available?</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|―――――――――――S24.4 - Else</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|―――――――――――――S24.5 - Unplug cable</td> <td>OK</td> <td>PASS</td> </tr> <tr> <td>|――――――――S7.2 Connect Media</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|―――――――――SUB25 - Connect Media</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|―――――――――――S25.1 - Is External Media Connect Available?</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|―――――――――――S25.4 - Else</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|―――――――――――――S25.5 - Plug cable</td> <td>OK</td> <td>PASS</td> </tr> <tr> <td>|――――――――S7.3 RegisterSession - Don't expect success</td> <td> </td> <td>N/A</td> </tr> <tr> <td>|―――――――――SUB3 - Register Session</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|―――――――――――S3.1 Register Session Try Loop</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|―――――――――――――S3.1 Register Session Try Loop[1]</td> <td bgcolor="lightgray"> </td> <td bgcolor="lightgray">SKIP</td> </tr> <tr> <td>|―――――――――――――――S3.1.1 RegisterSession</td> <td bgcolor="yellow"> Status 0x 00</td> <td>N/A</td> </tr> <tr> <td>|―――――――――――――――S3.1.2 Break out of loop if RegisterSession succeeded</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|―――――――――――――――S3.1.3 Else Notify that RegisterSession failed</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|―――――――――――――――――S3.1.3 TestNote</td> <td bgcolor="cyan">S3.1 RegisterSession attempt has failed (this behavior might be expected).</td> <td bgcolor="cyan">ADVISORY</td> </tr> <tr> <td>|――――――――S7.4 Get TCPIP status attribute</td> <td> Status 0x 00</td> <td>N/A</td> </tr> <tr> <td>|――――――――S7.5 If able to communicate...</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――――――S7.6 Turn off DHCP Server</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|―――――――――SUB20 - Stop DHCP Server</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|―――――Power Cycle</td> <td> </td> <td>N/A</td> </tr> <tr> <td>|――――――SUB4 - Cycle Power</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――――――S4.1 Ensure session is unregistered</td> <td></td> <td>N/A</td> </tr> <tr> <td>|――――――――S4.2 Power Off Command - External</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――――――S4.3 Power Off - Internal</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――――――――S4.3 Power Off</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――――――S4.4 Turn on DHCP Server, if needed</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|―――――――――SUB19 - Start DHCP Server</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――――――S4.5 Settling Time - External</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――――――S4.6 Settling Time - Internal</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――――――――S4.6.1 Power Off Settling Time</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――――――S4.7 Power On Command - External</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――――――S4.8 - Power On Internal</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――――――――S4.9 Power On</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――――――S4.4 Wait for Startup?</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――――――――S4.4.1 Startup Delay</td> <td>30000ms</td> <td>PASS</td> </tr> <tr> <td>|――――――――――S4.4.2 Stop DHCP Server</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|―――――――――――SUB20 - Stop DHCP Server</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|―――――Register Session</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――――SUB3 - Register Session</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――――――S3.1 Register Session Try Loop</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――――――――S3.1 Register Session Try Loop[1]</td> <td bgcolor="lightgray"> </td> <td bgcolor="lightgray">SKIP</td> </tr> <tr> <td>|――――――――――――S3.1.1 RegisterSession</td> <td></td> <td>N/A</td> </tr> <tr> <td>|――――――――――――S3.1.2 Break out of loop if RegisterSession succeeded</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――――――――――――BreakStep</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――――――S3.2 Check for failed RegisterSession</td> <td> </td> <td>PASS</td> </tr> <tr> <td bgcolor="red">|―――――3.8.2 Verify Last Conflict Detected</td> <td bgcolor="yellow"> </td> <td bgcolor="red">FAIL</td> </tr> <tr> <td bgcolor="red">|――――――SUB8 - Verify Last Conflict Detected</td> <td> </td> <td bgcolor="red">FAIL</td> </tr> <tr> <td>|――――――――S8.1 - Get TCPIP Attribute 11 Last Conflict Detected</td> <td>0200216C123456000108000604000100216C123456C0A8010A000000000000C0A8010A</td> <td>PASS</td> </tr> <tr> <td>|――――――――S8.2 - Get AcdActivity Byte</td> <td><hex>02</hex></td> <td>PASS</td> </tr> <tr> <td bgcolor="red">|――――――――S8.3 - Verify AcdActivity is 01</td> <td> </td> <td bgcolor="red">FAIL</td> </tr> <tr> <td bgcolor="red">|――――――――――SetFail</td> <td bgcolor="yellow"> LastConflictDetected: AcdActivity must be 01. </td> <td bgcolor="red">FAIL</td> </tr> <tr> <td>|――――――――S8.5 - Get Remote MAC</td> <td><hex>00216C123456</hex></td> <td>PASS</td> </tr> <tr> <td>|――――――――S8.6 - Verify Remote MAC</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――――――S8.7 - Get ARP PDU</td> <td><hex>000108000604000100216C123456C0A8010A000000000000C0A8010A</hex></td> <td>PASS</td> </tr> <tr> <td>|―――――3.8.3 Verify Arp Pdu matches what we sent</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|―――――3.8.4 Verify AcdStatus cleared</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――――SUB9 - Verify Status bits cleared</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――――――S9.1 - Get TCPIP Attribute 1</td> <td>01000000</td> <td>PASS</td> </tr> <tr> <td>|――――――――S9.2 - Mask bit 6 & bit 7 of Status Attribute</td> <td><hex>0000</hex></td> <td>PASS</td> </tr> <tr> <td>|――――――――S9.3 - Verify Status bits 6 & 7 are zero</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|―3.9 Attribute 11 reset via Type 1 Reset service to the Identity object</td> <td bgcolor="lightgray">*** SKIPPED ***</td> <td bgcolor="lightgray">SKIP</td> </tr> <tr> <td>|―4.1 No IP Frames Sent Until Address Successfully Probed</td> <td bgcolor="lightgray">*** SKIPPED ***</td> <td bgcolor="lightgray">SKIP</td> </tr> <tr> <td>|―4.2 ACD Probe Timing and ACD Announce Timing</td> <td bgcolor="lightgray">*** SKIPPED ***</td> <td bgcolor="lightgray">SKIP</td> </tr> <tr> <td>|―4.3 ACD Process Restarted When Cable Reconnected</td> <td bgcolor="lightgray">*** SKIPPED ***</td> <td bgcolor="lightgray">SKIP</td> </tr> <tr> <td>|―4.4 Ongoing ACD Probe Timing (10 minutes)</td> <td bgcolor="lightgray">*** SKIPPED ***</td> <td bgcolor="lightgray">SKIP</td> </tr> <tr> <td>|―4.5 Semi-Active State For Multi-Port Devices</td> <td bgcolor="lightgray">*** SKIPPED ***</td> <td bgcolor="lightgray">SKIP</td> </tr> <tr> <td>|―4.6 Multi-Port Devices Restart ACD Process on Link Up</td> <td bgcolor="lightgray">*** SKIPPED ***</td> <td bgcolor="lightgray">SKIP</td> </tr> <tr> <td>|―4.7 Conflict Detection During Probe Phase - ARP Announce</td> <td bgcolor="lightgray">*** SKIPPED ***</td> <td bgcolor="lightgray">SKIP</td> </tr> <tr> <td>|―4.8 Conflict Dection After Probe Phase</td> <td bgcolor="lightgray">*** SKIPPED ***</td> <td bgcolor="lightgray">SKIP</td> </tr> <tr> <td>|―4.9 Verify LastConflictDetected Attribute</td> <td bgcolor="lightgray">*** SKIPPED ***</td> <td bgcolor="lightgray">SKIP</td> </tr> <tr> <td>|―4.10 Conflict Isn't Detected Between Announce Frames</td> <td bgcolor="lightgray">*** SKIPPED ***</td> <td bgcolor="lightgray">SKIP</td> </tr> <tr> <td>|―4.11 ACD Defend</td> <td bgcolor="lightgray">*** SKIPPED ***</td> <td bgcolor="lightgray">SKIP</td> </tr> <tr> <td>|―4.12 Conflict After Successful Address Probe</td> <td bgcolor="lightgray">*** SKIPPED ***</td> <td bgcolor="lightgray">SKIP</td> </tr> <tr> <td>|―4.13 Address Not Used When Conflict is Declared</td> <td bgcolor="lightgray">*** SKIPPED ***</td> <td bgcolor="lightgray">SKIP</td> </tr> <tr> <td>|―4.14 Directed ARP During Probe Phase Does Not Cause Conflict</td> <td bgcolor="lightgray">*** SKIPPED ***</td> <td bgcolor="lightgray">SKIP</td> </tr> <tr> <td>|―4.15 Directed ARP Response In Ongoing Detection</td> <td bgcolor="lightgray">*** SKIPPED ***</td> <td bgcolor="lightgray">SKIP</td> </tr> <tr> <td>|―4.16 Conflict Detection During Probe Phase - ARP Probe</td> <td bgcolor="lightgray">*** SKIPPED ***</td> <td bgcolor="lightgray">SKIP</td> </tr> <tr> <td>FinallyRoutine</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|―FI - Final Power cycle DUT.</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――SUB4 - Cycle Power</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――S4.1 Ensure session is unregistered</td> <td></td> <td>N/A</td> </tr> <tr> <td>|――――S4.2 Power Off Command - External</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――S4.3 Power Off - Internal</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――――S4.3 Power Off</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――S4.4 Turn on DHCP Server, if needed</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|―――――SUB19 - Start DHCP Server</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――S4.5 Settling Time - External</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――S4.6 Settling Time - Internal</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――――S4.6.1 Power Off Settling Time</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――S4.7 Power On Command - External</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――S4.8 - Power On Internal</td> <td> </td> <td>PASS</td> </tr> <tr> <td>|――――――S4.9 Power On</td> <td> </td> <td>PASS</td> </tr> </table> </body> </html>
Regards
Andre
Thanks Andreas for the info, Our team is analyzing the info. Let me get back by Thursday on this.
One more issue:
If they test “Ethernet Link” case more than one time, this test case probably has error at switching between 10M and 100M.
When error occur, they can’t PING AM243-LP by computer anymore.
The test log and AM243 log are attached, and test result as below:
Regarding license issue, do you have feedback?
customer sometimes reproduce this issue in “Ethern
et Link” case:
Regards
Andre
log as attachmentsCT19_am243x-lp_tiEtherNetIP_freeRTOS.log
DMSC Firmware Version 8.5.3--v08.05.03 (Chill Capybar DMSC Firmware revision 0x8 DMSC ABI revision 3.1 [BOOTLOADER_PROFILE] Boot Media : NOR SPI FLASH [BOOTLOADER_PROFILE] Boot Media Clock : 100.000 MHz [BOOTLOADER_PROFILE] Boot Image Size : 875 KB [BOOTLOADER_PROFILE] Cores present : r5f0-0 [BOOTLOADER PROFILE] SYSFW init : 10850us [BOOTLOADER PROFILE] System_init : 5367701us [BOOTLOADER PROFILE] Drivers_open : 268us [BOOTLOADER PROFILE] Board_driversOpen : 153626us [BOOTLOADER PROFILE] Sciclient Get Version : 10022us [BOOTLOADER PROFILE] CPU load : 10945us [BOOTLOADER_PROFILE] SBL Total Time Taken : 184707us Image loading done, switching to application ... Pruicss max =3 selected PRU:3 Did Map 0x30080000 len 0x2000 to 0x30080000 (dram0) Did Map 0x30082000 len 0x2000 to 0x30082000 (dram1) Did Map 0x300b4000 len 0x4000 to 0x300b4000 (iram0) Did Map 0x300b8000 len 0x4000 to 0x300b8000 (iram1) Did Map 0x30090000 len 0x10000 to 0x30090000 (shdram) Did Map 0x300a2000 len 0x400 to 0x300a2000 (control0) Did Map 0x300a4000 len 0x400 to 0x300a4000 (control1) Did Map 0x300a0000 len 0x2000 to 0x300a0000 (intc) Did Map 0x300a6000 len 0x2000 to 0x300a6000 (cfg) Did Map 0x300a8000 len 0x2000 to 0x300a8000 (uart0) Did Map 0x300ae000 len 0x2000 to 0x300ae000 (iep) Did Map 0x300b0000 len 0x2000 to 0x300b0000 (ecap0) Did Map 0x300b2000 len 0x400 to 0x300b2000 (mii_rt) Did Map 0x300b2000 len 0x1c00 to 0x300b2000 (mdio) DP83869 detected DP83869 detected PRU_PHY_detect:181 Phy 3 alive PRU_PHY_detect:181 Phy 15 alive Phy 3 : Disable GBit ANEG Phy 15 : Disable GBit ANEG Phy 3 : RGMII enable low latency Phy 15 : RGMII enable low latency Phy 3 : RGMII set TX Half/Full Threshold: 1 Phy 15 : RGMII set TX Half/Full Threshold: 1 Phy 3 : RGMII set RX Half/Full Threshold: 1 Phy 15 : RGMII set RX Half/Full Threshold: 1 +EI_API_ADP_pruicssStart -EI_API_ADP_pruicssStart Local interface IP is 192.168.1.10 EI_API_ADP_getMacAddr: f4:84:4c:f9:8c:0a tcp_err_handler: Connection aborted. (-13) tcp_err_handler: Connection aborted. (-13)
hi Andrea,
thanks for the trace. We can now confirm that there is an issue in the ACD implementation. The problem with the failing conflict detection showed up when we migrated from the older 0.7 lwIP stack to the newer lwIP socket based interface between our version 1.04.10 (which had been ODVA certified with CT18.1) and version 2.01.00 which used the new interface between the EtherNet/IP stack and the lwIP stack.
We also looked though the SDK examples (08.04.00.17) . We don't see the reported error. The Wireshark trace you sent however clearly shows an issue the the conflict pretended by the conformance test tool is not detected.
In the trace that we produced here (with the TMDS64GPEVM) you see our ARP probe in Line 21 and the response from the tool in line 22 (23 is just a duplicate made up by Wireshark), and the next test case starts in line 27. So we are a bit puzzled concerning the results in your trace.
Hi Nilabh
Thanks for your support.
Our SDK version is 08.05.00.24. Does this version have the LwIP problem?
Is it a stack problem or an ODVA's problem?
By the way, Andre ever mentioned a version 8.6 will release to solve the “Profile verification” test fail issue. May I know when the version will be released?
What are the test issues that TI already knows on the CT19.1 of ODVA conformance test tool?
Best regards
Bo-Cheng
Hi Andrea/Bo-Cheng
As I mentioned before with our setup here we did not see this error messages. Therefore it would be important to exactly reproduce your setup.
We are trying to reproduce your setup on our side for this we need:
Nilabh,
Here is reply from customer:
Ethernet and app setting are as attachments. All are according to the instruction of the ODVA CT19.1 user manual. All firewalls are disabled in the test PC.
If other setting need to be confirmed?
Regards
Andre
Hello Nilabh,
Do you have any update?
By the way, do you have the schedule of when the stack V8.6 will release?
Thank you
Bo-Cheng
As I had requested I need the .out and .appimage file to reproduce the setup.
Could you please share that.
Customer's test image as attachment.
Regards
Andreethernetip_adapter_rgmii_demo_am243x-lp_r5fss0-0_freertos_ti-arm-clang.appimage
Thanks Andrea for sharing this.
I would also like to know is the usage of RGMII mode intentional, if yes may I know the reason?
We have earlier seen some instability with RGMII.
For the time being please use MII mode binaries to test/ Attaching the binaries.
/cfs-file/__key/communityserver-discussions-components-files/908/ti_2D00_arm_2D00_clang.7z
Nilabh,
Customer have test the MII mode with v8.5 stack on EVM: LP-AM243 / PROC109E2 (GP device).
The used .soc file and the UART output are also in attached.
Customer want to know,
Since the testing issues are happened on the evaluation board, such unstable and failure testing result is already affect the product development.
We hope the root cause can be figuring out as soon as possible.
Regards
Andre'
am243x-lp_tiEtherNetIP_freeRTOS.socCT19_am243x-lp_tiEtherNetIP_freeRTOS-5timesEthernetLinkTest.log
Hi Andrea,
I just got feedback from the development team. They use the appimage that you sent us and flashed it into a non HS_FS Launchpad. We had seen no error in the ACD test with this image. Attached you find the Log and the Wireshark trace.
Regards,
Martin
ACD full test report.zip
Martin,
Anything wrong with their setup? Can you please help to check anything different than our test setup so their result is bad ?
Regards
Andre
Hi Martin, Nilabh
Thank you for the ACD full test report. I have compared the report with ours, and I found our ARP Probe behaviors are very different then yours.
May I know what's the brand and model of hubs/switches did you use for the ACD tests?
Thank you
Bo-Cheng
Hi Bo-Cheng
Since our team is OOO next week, please expect a response by 19th June.
Hi Bo-Cheng
we use the following test setup as described in the conformance test example report (Excel)
The switch used by the tester is a tp-link TL-SG108PE.
Attached you find the test results obtained with an E2 revision launchpad.
ACD full test report_boardE2.zip
Regards,
Nilabh A.
Could you also please share your setup info, like the block diagram and the equipment's used.
Hi Nilabh,
Our ACD test setup is like the figure below.
I also tested with the I219-V newwork card, and the result was the same.
Regards
Bo-Cheng
Hi Bo-Cheng
We don't see anything that would explain they behavior they seem to see. There's one thing we haven't asked yet. The network traffic, are you recording it via a mirror port on the switch or directly on the network port on the test PC. The second thing that comes to our mind would be if you have checked the firewall logs. Possibly something got blocked there. Firewalls get picky when they see duplicate use of IP addresses.
Could you please check the above points?
Hi Andrea,
Could you please arrange a debug call with customer to look into this issue, We will have our team joint yeh call. Wednesday next week 21/06/23 seems to be good for us
I sent you web conference already, and I saw you accepted invitation last week.
Any issue???
Regards
Andre
Customer wants to discuss anther e2e issue which did not get any feedback in the past two weeks. https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/1232056/am2434-ethernet-ip-cip-motion-feature-support
Please also prepare the answer to address these issues in the meeting.
Regards
Andre
Customer wants to discuss anther e2e issue which did not get any feedback in the past two weeks. https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/1232056/am2434-ethernet-ip-cip-motion-feature-support
Please also prepare the answer to address these issues in the meeting.
Regards
Andre
Hi Nilabh,
Let me update a latest test result.
Best Regard
Bo-Cheng
Hello Nilabh,
May I ask for a WireShark data between the DUT and the Switch of the ACD behavior test 4.3?
I want to compare our behavior with yours.
Thank you
Bo-Cheng
Hi Bo-Cheng
We rerun now ACD tests on both LP-AM243 PROC109E2 (with our release 2.1 for SDK 08.05) and with the PROC109E3 HS_FS with the official MCU+ SDK 08.06.00.43. Attached you find the test results. We have not observed any issues. The error messages we had seen this morning on the E2 revision board was a typical 'Change User' scenario (i.e. change me), We just forgot to modify the MAC address in the SOC editor of the CT19.1. Once the correct MAC address is set in SOC editor (in the tool it's still call STC Editor) under 246Ethernet Link - Instance Group 1 and under Physical Data - TCP Interface 1, tests are running with result PASS.
There are however the know issues in the 08.06.00.43 release (calloc, time sync) that need an update.
best regards,
Martin
ACD Behavior Test V2.4.13 TC 4.3 Generic Device Port 1 LP-AM243 2023-07-05T15_MCU_PLUS_SDK_08.06.00.43.zipACD Behavior Test V2.4.13 TC 4.3 Generic Device Port 1 LP-AM243 2023-07-05T15_MCU_PLUS_SDK_08.05.00.01.zipACD Behavior Test V2.4.13 Run All Generic Device Port 1 LP-AM243 2023-07-05T15_MCU_PLUS_SDK_08.05.00.01.zip
May I ask for a WireShark data between the DUT and the Switch of the ACD behavior test 4.3?
I want to compare our behavior with yours.
LP-AM243_Interactive_ACD_Behavior_Test_V2.4.13_Test_section_4.3.pcapng.zip
Hello Nilabh,
Our Wireshark logs between the DUT and the swirch as attachment. One is tested with a PHOENIX CONTACT switch, and another is with a TP Link switch.
In the end of last week I got a TP Link switch TL-SG108E. I used it on the test 4.3, and the test is passed. However, as I know, ODVA use the D-Link DGS-1210-10P switch, not the TP-Link one. I ever used different switches for the test, but only the TP-Link can pass this test.
Could you ask KUNBUS to use other brand's switch for the ACD behavior test? In current situation, it's hard to have confidence that the product can pass the test at ODVA labs.
The list of switches we ever used:
1. D-Link DGS-12210-10MP (Fail)
2. D-Link DES1005A (Fail)
3. PHOENIX CONTACK FL SWITCH SFNB 5TX (Fail)
4. SIEMENS SCALANCE 204IRT (Fail)
5. HP (Fail)
6. TP-Link TL-SG108E (Pass)