Part Number: MSPM0L1303
We have a tech issue on the debugger, can you please check the below request
It seems like an issue with the debugger. It has occurred in 2 evaluation boards. When I try to go into the debugger mode, it is unable to connect to XDS emulator. Hence I am unable to flash and debug programs in the board. It would be great if you can help resolve this issue since I couldn’t find any working solution.
The error message reads:
Fatal Error: Failed to connect to the XDS emulator (connect CPU)
(Error -613 @ 0x0)
The target indicates that it is busy. Either try the SWD request again, or abort the transaction. (Emulation package 9.2.0.00002)
Thanks!
Frank