This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi experts,
I am working on the flash driver example (ospi_flash_io) using a LP-AM243 (E3) and MCU+SDK 08.05.00.24.
The example works fine for me as long as I execute it from RAM. As soon as I try to use it with XIP it doesn't work anymore.
Additional information: executing the flash driver example from RAM and just adding a MPU entry for XIP configuration will cause the example to get stuck or fail (the behaviour depends on the Access Permissions and Region Attributes MPU configuration in syscfg).
Thanks!
Best regards,
Jan
Hello Ming,
thanks for your fast response! Could you please clarify the following:
Thanks!
Best regards,
Jan
Hi Ming,
I see this differently looking at this AM243x MCU+ SDK 08.05.00: Enabling XIP or eXecute In Place
Can you comment?
Regards, Bernd
Hi Jan and Bo,
I am sorry for the incorrect answer provided in the previous post. In fact, the AM243x does support XIP from OSPI flash via FSS+OSPI controller.
Here is the XIP example in MCU+ SDK for AM243x 08.05.00.24: C:\ti\mcu_plus_sdk_am243x_08_05_00_24\examples\kernel\dpl\xip_benchmark.
You can also refer to the user guide at: AM243x MCU+ SDK: XIP Benchmark (ti.com)
I also noticed that the memory address for OSPI flash you used for "MPU region at start address 0x6000000 in syscfg" is incorrect. It should be 0x60000000.
Best regards,
Ming
Hi Ming,
customer has already verified that the XIP on the AM24 is working in principle. In conjunction with the Flash driver, it has not worked yet, so the following questions remain:
Regards, Bernd
Hi Bo,
First of all, if the flash driver is in the flash, how can the flash be initialized first time? If the flash cannot be initialized , then how the code be XIPed from flash. The simple answer is the "Executing the flash driver itself from flash" is not possible.
On the other hand, "Executing the flash driver from RAM while other code parts are executed from flash" is possible, but the performance may not be ideal.
Best regards,
Ming
Hi Ming,
the answer is sufficient at this point for the time being. If more questions arise on this topic, I will come back more specifically.
Regards, Bernd