This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Now we need use SafeTI diagnostic library to executes CPU Logic Built-In Self Test using Self-Test Controller for RM57Lx MCU.
But I don't find related example code in Demo_app project, can you procide the example code for below test types with API SL_SelfTest_STC and SL_SelfTest_Status_STC?
Thanks so much!
Hi Jagadish,
I know where to find the API funtion, but I don't know how to call it and how to construct the stcSelfTestConfig struct as a input parameter?
The below example is just a interface description and it's not for RM57Lx.
Hi Shenruming,
I know where to find the API funtion, but I don't know how to call it and how to construct the stcSelfTestConfig struct as a input parameter?
Please refer below two highlighted lines to understand the calling procedure.
--
Thanks & regards,
Jagadish.
Hi Jagadish,
Thanks for your great support!
It's about STC selfcheck. How about CPU test using STC1_RUN/STC2_RUN?
Hi Shenruming,
It's about STC selfcheck. How about CPU test using STC1_RUN/STC2_RUN?
My first image shows for calling procedure for STC1_RUN right?
And for STC2_RUN and STC2_COMPARE_SELFCHECK just change the corresponding macros and procedure was same.
--
Thanks & regards,
Jagadish.
Hi Jagadish,
I can't get the whole code about STC1_RUN/STC2_RUN test. Can you send me the HL_sys_startup.c or attach the complete code including parameter preparing, test result handling etc.?
STC RUN test on startup is very important for us.
Thanks so much!
Hi Shenruming,
/** @file HL_sys_startup.c * @brief Startup Source File * @date 02-Mar-2016 * @version 04.05.02 * * This file contains: * - Include Files * - Type Definitions * - External Functions * - VIM RAM Setup * - Startup Routine * . * which are relevant for the Startup. */ /* * Copyright (C) 2009-2016 Texas Instruments Incorporated - www.ti.com * * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the * distribution. * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. * */ /* USER CODE BEGIN (0) */ /* USER CODE END */ /* Include Files */ #include "HL_sys_common.h" #include "HL_system.h" #include "HL_sys_vim.h" #include "HL_sys_core.h" #include "HL_esm.h" #include "HL_sys_mpu.h" /* USER CODE BEGIN (1) */ #include "HL_sys_selftest.h" #include "esm_application_callback.h" #include "sl_priv.h" /* USER CODE END */ /* USER CODE BEGIN (2) */ volatile uint64 crcAtInit_VIMRAM = 0; volatile uint64 crcAtInit_FLASH = 0; /* USER CODE END */ /* External Functions */ /*SAFETYMCUSW 218 S MR:20.2 <APPROVED> "Functions from library" */ extern void __TI_auto_init(void); /*SAFETYMCUSW 354 S MR:NA <APPROVED> " Startup code(main should be declared by the user)" */ extern void main(void); /*SAFETYMCUSW 122 S MR:20.11 <APPROVED> "Startup code(exit and abort need to be present)" */ /*SAFETYMCUSW 354 S MR:NA <APPROVED> " Startup code(Extern declaration present in the library)" */ extern void exit(int _status); /* USER CODE BEGIN (3) */ void afterSTC(void); SL_ResetReason resetReason; /* Reset reason */ /* USER CODE END */ /* Startup Routine */ void _c_int00(void); /* USER CODE BEGIN (4) */ extern uint32 ulHighHandlerLoadStart; extern uint32 ulHighHandlerLoadEnd; extern uint32 ulHighHandlerSize; extern uint32 ulHighHandlerStartAddr; extern uint32 ulHighHandlerEndAddr; SL_STC_Config stcSelfTestConfig; /* STC Configuration */ /* USER CODE END */ #pragma CODE_STATE(_c_int00, 32) #pragma INTERRUPT(_c_int00, RESET) #pragma WEAK(_c_int00) void _c_int00(void) { /* USER CODE BEGIN (5) */ #if 0 /* USER CODE END */ /* Initialize Core Registers to avoid CCM Error */ _coreInitRegisters_(); /* Reset handler: the following instructions read from the system exception status register * to identify the cause of the CPU reset. */ switch(getResetSource()) { case POWERON_RESET: case DEBUG_RESET: case EXT_RESET: /* USER CODE BEGIN (6) */ #endif /* Initialize Core Registers to avoid CCM Error */ SL_Init_R5Registers(); /* Initialize Stack Pointers * The SL_Init_ResetReason API (and the correspondig HALCoGen getresetsource API) is a C function which uses stack. * Stack must be setup correctly before calling this function.*/ SL_Init_StackPointers(); /* Enable CPU Event Export */ /* This allows the CPU to signal any single-bit or double-bit errors detected * by its ECC logic for accesses to program flash or data RAM. */ /* NOTE - needs to be called on every reset */ _SL_Init_EnableEventExport(); resetReason = SL_Init_ResetReason(); switch(resetReason) { case RESET_TYPE_POWERON: case RESET_TYPE_DEBUG: case RESET_TYPE_EXTRST: case RESET_TYPE_EXTRST_NERROR: #if 0 /* USER CODE END */ /* Initialize L2RAM to avoid ECC errors right after power on */ _memInit_(); /* USER CODE BEGIN (7) */ #endif /* Initialize L2RAM to avoid ECC errors right after power on * This function uses the system module's hardware for auto-initialization of memories and their * associated protection schemes. The CPU RAM is initialized by setting bit 0 of the MSIENA register. * Hence the value 0x1 passed to the function. * This function will initialize the entire CPU RAM and the corresponding ECC locations. */ SL_Init_Memory(RAMTYPE_RAM); /* USER CODE END */ /* USER CODE BEGIN (8) */ #if 0 /* USER CODE END */ /* Initialize Stack Pointers */ _coreInitStackPointer_(); /* USER CODE BEGIN (9) */ #endif #if 0 /* USER CODE END */ /* Enable CPU Event Export */ /* This allows the CPU to signal any single-bit or double-bit errors detected * by its ECC logic for accesses to program flash or data RAM. */ _coreEnableEventBusExport_(); /* USER CODE BEGIN (10) */ #endif /* Enable CPU Event Export */ /* This allows the CPU to signal any single-bit or double-bit errors detected * by its ECC logic for accesses to program flash or data RAM. */ //_SL_Init_EnableEventExport(); /* USER CODE END */ /* Check if there were ESM group3 errors during power-up. * These could occur during eFuse auto-load or during reads from flash OTP * during power-up. Device operation is not reliable and not recommended * in this case. */ if ((esmREG->SR1[2]) != 0U) { while(1); //ESM group3 error } /* Initialize System - Clock, Flash settings with Efuse self check */ systemInit(); /* USER CODE BEGIN (11) */ #if 0 /* USER CODE END */ /* Enable IRQ offset via Vic controller */ _coreEnableIrqVicOffset_(); /* Initialize VIM table */ vimInit(); /* USER CODE BEGIN (12) */ /* USER CODE END */ /* Configure system response to error conditions signaled to the ESM group1 */ /* This function can be configured from the ESM tab of HALCoGen */ esmInit(); /* USER CODE BEGIN (13) */ #endif #if 0 /* USER CODE END */ break; case OSC_FAILURE_RESET: /* USER CODE BEGIN (14) */ #endif break; case RESET_TYPE_OSC_FAILURE: #if 0 /* USER CODE END */ break; case WATCHDOG_RESET: /* USER CODE BEGIN (15) */ #endif break; case RESET_TYPE_WATCHDOG: #if 0 /* USER CODE END */ break; case CPU0_RESET: case CPU1_RESET: /* USER CODE BEGIN (16) */ #endif break; case RESET_TYPE_CPU0: case RESET_TYPE_CPU1: /* Reset caused due to CPU reset. CPU reset can be caused by CPU self-test completion, or by toggling the "CPU RESET" bit of the CPU Reset Control Register. */ /* reset could be caused by stcSelfCheck run or by an actual CPU self-test run */ /* check if this was an stcSelfCheck run */ #if defined(_TMS570LS31x_) || defined(_TMS570LS12x_) || defined(_RM48x_) || defined(_RM46x_) || defined(_RM42x_) || defined(_TMS570LS04x_) if ((stcREG->STCSCSCR & 0xFU) == 0xAU) { /* check if the self-test fail bit is set */ if ((stcREG->STCGSTAT & 0x3U) != 0x3U) #endif #if defined(_TMS570LC43x_) || defined(_RM57Lx_) if ((stcREG1->STCSCSCR & 0xFU) == 0xAU) { /* check if the self-test fail bit is set */ if ((stcREG1->STCGSTAT & 0x3U) != 0x3U) #endif { for(;;) { } } /* STC self-check has passed */ else { /* clear self-check mode */ #if defined(_TMS570LS31x_) || defined(_TMS570LS12x_) || defined(_RM48x_) || defined(_RM46x_) || defined(_RM42x_) || defined(_TMS570LS04x_) stcREG->STCSCSCR = 0x05U; /* clear STC global status flags */ stcREG->STCGSTAT = 0x3U; #endif #if defined(_TMS570LC43x_) || defined(_RM57Lx_) stcREG1->STCSCSCR = 0x05U; /* clear STC global status flags */ stcREG1->STCGSTAT = 0x3U; #endif /* clear ESM group1 channel 27 status flag */ esmREG->SR1[0U] = 0x08000000U; /* Start CPU Self-Test */ /*there is no alternate usercode place holder to place the safety library api so this block of code can * get overwritten on helcogen code regeneration*/ /*********************************************************************************************************/ /*cpuSelfTest(STC_INTERVAL, STC_MAX_TIMEOUT, TRUE);*/ stcSelfTestConfig.stcClockDiv = 0; /* STC Clock divider = 1 */ stcSelfTestConfig.intervalCount = 1; /* One interval only */ stcSelfTestConfig.restartInterval0 = TRUE; /* Start from interval 0 */ stcSelfTestConfig.timeoutCounter = 0xFFFFFFFF; /* Timeout counter*/ _SL_HoldNClear_nError(); /* mask vim interrupts before running STC */ vimREG->REQMASKCLR0 = 0xFFFFFFFFu; vimREG->REQMASKCLR1 = 0xFFFFFFFFu; vimREG->REQMASKCLR2 = 0xFFFFFFFFu; vimREG->REQMASKCLR3 = 0xFFFFFFFFu; /* ensure no pending ESM GRP2 errors before running STC */ if(esmREG->SSR2 == 0u) #if defined(_TMS570LS31x_) || defined(_TMS570LS12x_) || defined(_RM48x_) || defined(_RM46x_) || defined(_RM42x_) || defined(_TMS570LS04x_) {SL_SelfTest_STC(STC_RUN, TRUE, &stcSelfTestConfig);} #endif #if defined(_TMS570LC43x_) || defined(_RM57Lx_) {SL_SelfTest_STC(STC1_RUN, TRUE, &stcSelfTestConfig);} #endif /*********************************************************************************************************/ } } /* CPU reset caused by CPU self-test completion */ #if defined(_TMS570LS31x_) || defined(_TMS570LS12x_) || defined(_RM48x_) || defined(_RM46x_) || defined(_RM42x_) || defined(_TMS570LS04x_) else if ((stcREG->STCGSTAT & 0x1U) == 0x1U) { /* Self-Test Fail flag is set */ if ((stcREG->STCGSTAT & 0x2U) == 0x2U) { #endif #if defined(_TMS570LC43x_) || defined(_RM57Lx_) else if ((stcREG1->STCGSTAT & 0x1U) == 0x1U) { /* Self-Test Fail flag is set */ if ((stcREG1->STCGSTAT & 0x2U) == 0x2U) { #endif for(;;) { } } /* CPU self-test completed successfully */ else { /* clear STC global status flag */ stcREG1->STCGSTAT = 0x1U; /* Continue start-up sequence after CPU STC completed */ afterSTC(); } } /* CPU reset caused by software writing to CPU RESET bit */ else { /* Add custom routine here to handle the case where software causes CPU reset */ /* USER CODE END */ /* USER CODE BEGIN (17) */ #if 0 /* USER CODE END */ /* Initialize Stack Pointers */ _coreInitStackPointer_(); /* USER CODE BEGIN (18) */ #endif #if 0 /* USER CODE END */ /* Enable CPU Event Export */ /* This allows the CPU to signal any single-bit or double-bit errors detected * by its ECC logic for accesses to program flash or data RAM. */ _coreEnableEventBusExport_(); /* USER CODE BEGIN (19) */ #endif /* Enable CPU Event Export */ /* This allows the CPU to signal any single-bit or double-bit errors detected * by its ECC logic for accesses to program flash or data RAM. */ _SL_Init_EnableEventExport(); #if 0 /* USER CODE END */ break; case SW_RESET: /* USER CODE BEGIN (20) */ #endif } break; case RESET_TYPE_SWRST: break; case RESET_TYPE_ICSTRST: if(!SL_SelfTest_Status_MemIntrcntSelftest()) { while(1); } //Memory Interconnect Error /* USER CODE END */ break; default: /* USER CODE BEGIN (21) */ /* USER CODE END */ break; } /* USER CODE BEGIN (22) */ if(RESET_TYPE_DEBUG != resetReason) { if(RESET_TYPE_ICSTRST != resetReason) { /* Memory interconnect selftest */ SL_SelfTest_MemoryInterconnect(MEMINTRCNT_SELFTEST); } /* Make sure that the CPU self-test controller can actually detect a fault inside CPU */ stcSelfTestConfig.stcClockDiv = 0; /* STC Clock divider = 1 */ stcSelfTestConfig.intervalCount = 1; /* One interval only */ stcSelfTestConfig.restartInterval0 = TRUE; /* Start from interval 0 */ stcSelfTestConfig.timeoutCounter = 0xFFFFFFFF; /* Timeout counter*/ _SL_HoldNClear_nError(); /* mask vim interrupts before running STC */ vimREG->REQMASKCLR0 = 0xFFFFFFFFu; vimREG->REQMASKCLR1 = 0xFFFFFFFFu; vimREG->REQMASKCLR2 = 0xFFFFFFFFu; vimREG->REQMASKCLR3 = 0xFFFFFFFFu; /* ensure no pending ESM GRP2 errors before running STC */ if(esmREG->SSR2 == 0u) { SL_SelfTest_STC(STC1_COMPARE_SELFCHECK, TRUE, &stcSelfTestConfig); } else { SL_SelfTest_STC(STC1_COMPARE_SELFCHECK, TRUE, &stcSelfTestConfig); } } else { afterSTC(); } } void afterSTC(void) { /* Enable IRQ offset via Vic controller */ _coreEnableIrqVicOffset_(); /* Initialize VIM table */ vimInit(); /* Configure system response to error conditions signaled to the ESM group1 */ /* This function can be configured from the ESM tab of HALCoGen */ esmInit(); /* USER CODE END */ _mpuInit_(); /* USER CODE BEGIN (23) */ /* USER CODE END */ _cacheEnable_(); /* USER CODE BEGIN (24) */ /* USER CODE END */ /* USER CODE BEGIN (25) */ /* USER CODE END */ /* initialize global variable and constructors */ __TI_auto_init(); /* USER CODE BEGIN (26) */ /* Initialize EPC */ epcInit(); /* enable DMA ECC */ sl_dmaREG->DMAPCR |= (uint32)0xAU; /* initialise DMA RAM */ SL_Init_Memory(RAMTYPE_DMA_RAM); /* Initialise ADC */ adcInit(); /* Initialise ADC SRAM */ SL_Init_Memory(RAMTYPE_MIBADC1_RAM); SL_Init_Memory(RAMTYPE_MIBADC2_RAM); /* Initialise MIBSPI */ mibspiInit(); /* Initialise MIBSPI SRAM */ SL_Init_Memory(RAMTYPE_MIBSPI1_RAM); SL_Init_Memory(RAMTYPE_MIBSPI2_RAM); SL_Init_Memory(RAMTYPE_MIBSPI3_RAM); SL_Init_Memory(RAMTYPE_MIBSPI4_RAM); SL_Init_Memory(RAMTYPE_MIBSPI5_RAM); /* Initialise SCI */ sciInit(); /* Initialise CAN */ canInit(); /* Initialise CAN SRAM */ SL_Init_Memory(RAMTYPE_DCAN1_RAM); SL_Init_Memory(RAMTYPE_DCAN2_RAM); SL_Init_Memory(RAMTYPE_DCAN3_RAM); SL_Init_Memory(RAMTYPE_DCAN4_RAM); SL_ESM_Init(ESM_ApplicationCallback); _enable_interrupt_(); uint32 i; uint32 size=(uint32)&ulHighHandlerSize; for(i=0;i<size;i++) { ((char *)&ulHighHandlerStartAddr)[i] =((char *)&ulHighHandlerLoadStart)[i]; } /* Boot time MIBSPI Analog Loopback Test */ SL_SelfTest_MibSPI(MIBSPI_ANALOG_LOOPBACK_TEST,SL_MIBSPI2); SL_SelfTest_MibSPI(MIBSPI_ANALOG_LOOPBACK_TEST,SL_MIBSPI4); SL_SelfTest_MibSPI(MIBSPI_ANALOG_LOOPBACK_TEST,SL_MIBSPI3); SL_SelfTest_MibSPI(MIBSPI_ANALOG_LOOPBACK_TEST,SL_MIBSPI1); SL_SelfTest_MibSPI(MIBSPI_ANALOG_LOOPBACK_TEST,SL_MIBSPI5); //Boot time Software test of VIM functionality SL_SelfTest_VIM(VIM_SOFTWARE_TEST); //Boot time Software test of DMA functionality SL_SelfTest_DMA(DMA_SOFTWARE_TEST); checkPLL1Slip(); checkPLL2Slip(); /* USER CODE END */ /* call the application */ /*SAFETYMCUSW 296 S MR:8.6 <APPROVED> "Startup code(library functions at block scope)" */ /*SAFETYMCUSW 326 S MR:8.2 <APPROVED> "Startup code(Declaration for main in library)" */ /*SAFETYMCUSW 60 D MR:8.8 <APPROVED> "Startup code(Declaration for main in library;Only doing an extern for the same)" */ main(); /* USER CODE BEGIN (27) */ /* USER CODE END */ /*SAFETYMCUSW 122 S MR:20.11 <APPROVED> "Startup code(exit and abort need to be present)" */ exit(0); /* USER CODE BEGIN (28) */ /* USER CODE END */ } /* USER CODE BEGIN (29) */ /* USER CODE END */ /* USER CODE BEGIN (30) */ /* USER CODE END */
Actually, after STC test the CPU will get reset and the below highlighted code is the test result handling
--
Thanks & regards.
Jagadish.
Hi Jagadish,
Thanks for your great help!
1.As we know, the debug starts from main function, but you put the STC test before main function in _c_int00.
How to debug the STC selftest funtion?
2. After error forcing test by runnging "SL_SelfTest_STC" with parameter "STC1_COMPARE_SELFCHECK", where did you running "SL_SelfTest_Status_STC" to get the test result?
3. STC1_COMPARE_SELFCHECK is a fault injection test, so it should be executed in case of need, but not be executed routinely.
So when will the test be started in below code? What's the triggering condition?
4. If we use your _c_int00 to replace the previous _c_int00 to do STC test, there's a big difference between them to be treated with caution:
You use the safety library to get the reset reason and the previous code use HalGOGEN functions to get the reset source.
Are they equivalent? Can we use your solution to replace the previous solution for business application? Thanks a lot!!
5. What's the treatment for "STC2_RUN" and "STC2_COMPARE_SELFCHECK"? No test cases for them.
I would greatly appreciate if you could reply to me one by one!!
Hi Shenruming,
1.As we know, the debug starts from main function, but you put the STC test before main function in _c_int00.
How to debug the STC selftest funtion?
The debug starts at main because of the following setting,
Here we gave Auto run to the main function right, that is why debug starts at main function. You can just give the required function where you want to start the debug.
Hi Jagadish,
Could you please answer the other 4 questions as well? They also seriously confuse us. Thanks.
Hi Shenruming,
Apologies for the delay, i am on vacation for few days.
2. After error forcing test by runnging "SL_SelfTest_STC" with parameter "STC1_COMPARE_SELFCHECK", where did you running "SL_SelfTest_Status_STC" to get the test result?
Actually, we can call the "SL_SelfTest_Status_STC" to get the test result if we are using SL_SelfTest_STC in our application but here in diagnostic they are directly verifying the result without calling the SL_SelfTest_Status_STC function as shown below
3. STC1_COMPARE_SELFCHECK is a fault injection test, so it should be executed in case of need, but not be executed routinely.
So when will the test be started in below code? What's the triggering condition?
In diagnostic library it is not executing routinely, as the code highlighted is located in the "_c_int00" function, it is executing only after each reset and except that reset is due to debug.
4. If we use your _c_int00 to replace the previous _c_int00 to do STC test, there's a big difference between them to be treated with caution:
You use the safety library to get the reset reason and the previous code use HalGOGEN functions to get the reset source.
Are they equivalent? Can we use your solution to replace the previous solution for business application? Thanks a lot!!
We can't use both interchangeably because both have different return values.
For example:
The below are the return values for the "getResetSource"
The below are the return values for the "SL_Init_ResetReason"
--
Thanks & regards,
Jagadish.