This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MCU-PLUS-SDK-AM243X: AM243x SDK N21 pin cannot find offset in pinmux.h file.

Expert 2891 points
Part Number: MCU-PLUS-SDK-AM243X
Other Parts Discussed in Thread: SYSCONFIG

Hi

My customer is developing AM243x.

In pin setting, want to set N21 pin to GPIO by sysconfig.

(I tested in Sysconfig 1.14.0, MCU+SDK 8.5.0.24, CCSVersion: 12.0.0.00009 )

But there was build error by undefined PIN_OSPI0_LBCLKO.

In SDK driver (mcu_plus_sdk_am243x_08_05_00_24\source\drivers\pinmux\am64x_am243x/pinmux.h), there is not define of N21 pinname (PIN_OSPI0_LBCLKO).

Is this bug?

--genereted file by sysconfig--

------
supplement:

In cloud sysconfig using PDK, (File name is AM243x_ALV_pinmux.h)

There was define of N21 pin name.

Thanks,

GR

  • Hi GR,

    It is a bug. The PIN_OSPI0_LBCLKO should have been included in the source\drivers\pinmux\am64x_am243x/pinmux.h. I will file JIRA ticket for this.

    Meanwhile, as a workaround, you can add the following line into the Pinmux_MainOffsets of source\drivers\pinmux\am64x_am243x/pinmux.h:

    PIN_OSPI0_LBCLKO = 0x0004,

    Best regards,

    Ming

  • Hi Ming,

    Thank you to your support.

    I will add the line.

    Best regards,

    GR