Part Number: LP-AM243
Other Parts Discussed in Thread: SYSCONFIG
Hello,
I'm trying to understand the implementation of the LP-AM243 QSPI and how it adheres to Errata i2307. The LP has implemented External Board Loopback. The "Workaround" in i2307 says that the "design must not use External Board Loopback if planning to use OSPI as a boot source." I understand that the Boot ROM only uses internal loopback and that other clock topologies can be used after boot.
I'd like clarification on "must not use External Board Loopback" because the LP-AM243 has apparently been implemented with it.
Has the LP-AM243 been able to get around this requirement by ensuring the propagation delay of OSPI0_Clk is <450pS?

Lastly, does Errata i2189 come into play with External Board Loopback because LBCLK routes into DQS? Or does it only apply to true DQS Mode combined with Octal SPI Flash containing a DQS Output?
Thanks very much,
Joe