Part Number: MCU-PLUS-SDK-AM263X
Hi, I have an application where I'd like to use three ethernet interfaces on an AM263x. I can use the CPSW3G for two of them, and I'd like to use the PRU-ICSS for the third one.
I see in the 9.0.0 version of MCU+SDK docs and syscfg that it appears the ENET-LLD driver supports only the CPSW peripheral (and not the ICSS).
However I see some source files that look like they're related to ENET-LLD implementation on ICSS (source/networking/enet/core/src/per/icssg.c) and older MCU+SDK versions (8.6.0) I saw references to the Enet-LLD supporting both peripherals:
Enet LLD supports two families of Ethernet devices: CPSW and ICSSG.
Could I have a TI recommendation as to whether it is possible to use the ENET-LLD driver with the AM263 PRU-ICSS peripheral with MCU+SDK/syscfg out of the box or with a reasonable amount of software work done by me?