Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MCU-PLUS-SDK-AM243X: EtherNet/IP Adapter API: NS Status in Bootp mode

Part Number: MCU-PLUS-SDK-AM243X

I built the demo below and checked its operation.

"ethernetip_adapter_generic_device_mii_demo_am243x-lp_r5fss0-0_freertos_ti-arm-clang"

We checked with version 09.00.00.03 of INDUSTRIAL-COMMUNICATIONS-SDK-AM243X.

I have a question regarding the behavior of the following API.

ETHIP_API uint32_t EI_API_ADP_setModuleNetworkStatusFunc(T* pAdp_p, EI_API_ADP_CBStatus callback_p)

This API allows you to specify a callback function to be called when the Module Status or Network Status changes.

However, the values that can be obtained using the callback function when an IP address has not been obtained are different between DHCP and Bootp.

If an IP address cannot be obtained using DHCP, EI_API_ADP_eSTATUS_LED_ALL_OFF can be obtained for Network Status "net".

However, in the case of Bootp, if the IP address cannot be obtained, EI_API_ADP_eSTATUS_LED_GREEN_BLINK can be obtained for Network Status "net".

I think the correct behavior is for Bootp to be able to obtain EI_API_ADP_eSTATUS_LED_ALL_OFF in the same way as DHCP when an IP address cannot be obtained.

Will it be fixed in the next update?