Part Number: MSPM0G3507
Hi
We are using the MSPM0G3507 in a new product and facing some issues.
We use the comparator module in the microcontroller to detect a current. If the current defined by the DAC12 is exceeded, a PWM timer is triggered (load event) trough the event system.
The concept works well so far, but there is a sporadic error that the output of the comparator reacts but no event is generated. The occurrence was reduced by activating the analog filter in the comparator. However, it seems that it can happen that the timer is not triggered.
Measurement:

Yellow: Comparator Input (Current Measurement)
Red: Comparator Output (Falling Edge produces Event)
Blue: PWM generated by Timer (high voltage side)
DAC12 not displayed.
Important note: We are using a pre-production microcontroller with part number: XMSM0G3507SPT
Can anyone help? Do you need additional informations?
Thank you.
Best regards
Dominik Wuest