This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Hercules TMDXRM57LHDK Dev Kit Rev E Populated pins for SCI and SPI Schematic/Manual

Part Number: TMDXRM57LHDK

Hello,

We are using the Hercules TMDXRM57LHDK Dev Kit Rev E.  Where can I find the info for what populated pins for SCI and SPI Schematic/Manual we can access on your Hercules board? Specifically SCI2, SCI3, SPI1 and SPI5 right now. I could see LIN1RX printed on back of board but not find corresponding TX pin and could not find the SCI2 for example. another example on front of the board with populated connector on the back a pin  is printed as T5, but on the back the same pin  shows it  as D13 is printed on the Rev E board (in case that was printed wrong on the Rev E version of the boards).  Is there a schematic for manual that lists the Hercules board pin mappings for the populated pins for your Rev E board?  Thank you.