Part Number: TIDEP-01032
Hi there!
Re documentation says that a "BLY342D-48V-3200" from Anaheim shall be used for the TIDEP-01032.
This is a 48V motor but the Booster pack AM2BLDCSERVO is rated only at 24V.
Can a 24V motor be used also?
Which are the key values for a different motor to be used for the TIDEP-01032? Anaheim is a little far fetched from Europe :)
rgds