Part Number: TMS570LC4357
Hello experts,
We are having some issues with the MEM8A: Boot Time Execution of Interconnect Self-Test and CPU2A: Boot Time Execution of LBIST STC diagnostics.
Both implementations worked fine initially, but now the tests seem to stop when the WFI instruction is reached.
Once the WFI instruction is reached, the SW stops responding. The expected CPU reset is not triggered.
As far as I understand, this can only happen if the WFI instruction is triggered, but the self test does not start.
So my question is: what could be preventing the WFI instruction from being properly executed?
Thank you and best regards,
Max