This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hii,
I am sampling adc sine wave ( soc from software ) with amplitude(high=1v and low=0v) with frequency of 1mhz but i am getting digital value between 2300 and 2450 . i should be gettiing from 0 to something?
what can be possible error??
The Start Of Conversion (SOC) is mostly configured in SYSCONFIG. Study the examples in combination with the TRM.
In Start Of Conversion(SOC) from software, are SYSCLK, ADC Clock Prescaler and SOCx Sample Window are enough for setting the sampling rate or do we need to initialize other driver like EPWM, because example in sdk for SOC from Software is only using SYSCLK for time reference for adc ??
The ADC can be triggered in many different ways as mentioned in the manual:
EPWM is just one option. The readme for your example is clear enough I think.
In this case, the sample rate is the rate at which ADC_forceSOC() is called:
hii kier,
I am using a sampling rate of greater than 3 msps ( SysClk=200MHz AdcClock=200/3 MHz ).
I am feeding the square wave of 1MHz to the J1/J3 Pin 23 of am2634 launchpad in Continuous mode but still i am getting data in range 1200 to 1400.
This is code for taking the digital data in SOC from Software.
while(1)
{
ADC_clearInterruptStatus(baseAddr, ADC_INT_NUMBER1);
ADC_forceSOC(baseAddr, ADC_SOC_NUMBER0);
while(ADC_getInterruptStatus(baseAddr, ADC_INT_NUMBER1) == false)
{
}
DebugP_log("ADC Result register value : %d\r\n", ADC_readResult(CONFIG_ADC0_RESULT_BASE_ADDR, ADC_SOC_NUMBER0));
}
pls suggest how to fix it.
When you say "fix it", you mean you want to achieve a sample rate of 4MSPS such that you can reliably reconstruct a 1MHz sine wave?
When you say "i am getting data", how are you viewing this data?
If you are just using the code above then the sample rate is only as fast as the call to ADC_forceSOC(). One of the problems could be that DebugP_log is a very slow process so the call frequency of ADC_forceSOC() will be low I imagine.
Comment out DebugP_log() and instead set-up a buffer to store the return value of ADC_readResult() but you will need quite a lot of memory. Then use the Graph feature to plot the data points:
Sorry but I'm not TI support staff so cannot afford to spend much more time on this. Hopefully TI will pick up this topic.
Hello Tej_1441, Kier,
I'll start by giving Kier a great Thank You for providing great initial feedback here.
I am glad to continue further support as needed.
Tej, where are you at now with your project?
Best Regards,
Zackary Fleenor
Based on the information I have gathered so far; I think a signal conditioning circuit needs to be included in the test setup. What instrumentation is being used to inject the 1 MHz sine wave? It will need sufficient drive strength to charge the S&H capacitor. The following app note is also applicable to the AM263x SAR ADC.
Hii Fleenor,
sorry for late reply as i was busy with some other works.
i have planned to do adc sampling with epwm as the trigger source for SOC, But even with this case i am stuck in similar situation, where i am able to sample signal of sine wave(amplitude 1VPP and offset 0.5V) till 50 KHz but when i increase frequency of signal then it is getting distorted and upper and lower values missing.
GRAPH at 150KHz.
Here is code for initilization of adc and epwm driver.
#include "ti_drivers_open_close.h" #include <kernel/dpl/DebugP.h> void Drivers_open(void) { Drivers_adcOpen(); Drivers_epwmOpen(); Drivers_intXbarOpen(); Drivers_uartOpen(); } void Drivers_close(void) { Drivers_uartClose(); } void Drivers_adcOpen() { /* CONFIG_ADC1 initialization */ /* Configures the analog-to-digital converter module prescaler. */ ADC_setPrescaler(CONFIG_ADC1_BASE_ADDR, ADC_CLK_DIV_3_0); /* Configures the analog-to-digital converter resolution and signal mode. */ ADC_setMode(CONFIG_ADC1_BASE_ADDR, ADC_RESOLUTION_12BIT, ADC_MODE_SINGLE_ENDED); /* Sets the priority mode of the SOCs. */ ADC_setSOCPriority(CONFIG_ADC1_BASE_ADDR, ADC_PRI_ALL_ROUND_ROBIN); /* Start of Conversion 0 Configuration */ /* Configures a start-of-conversion (SOC) in the ADC. */ ADC_setupSOC(CONFIG_ADC1_BASE_ADDR, 0, ADC_TRIGGER_EPWM0_SOCA, ADC_CH_ADCIN0, 16); /* Configures the interrupt SOC trigger of an SOC. */ ADC_setInterruptSOCTrigger(CONFIG_ADC1_BASE_ADDR, 0, ADC_INT_SOC_TRIGGER_NONE); /* Start of Conversion 1 Configuration */ /* Configures a start-of-conversion (SOC) in the ADC. */ ADC_setupSOC(CONFIG_ADC1_BASE_ADDR, 1, ADC_TRIGGER_SW_ONLY, ADC_CH_ADCIN0, 16); /* Configures the interrupt SOC trigger of an SOC. */ ADC_setInterruptSOCTrigger(CONFIG_ADC1_BASE_ADDR, 1, ADC_INT_SOC_TRIGGER_NONE); /* Start of Conversion 2 Configuration */ /* Configures a start-of-conversion (SOC) in the ADC. */ ADC_setupSOC(CONFIG_ADC1_BASE_ADDR, 2, ADC_TRIGGER_SW_ONLY, ADC_CH_ADCIN0, 16); /* Configures the interrupt SOC trigger of an SOC. */ ADC_setInterruptSOCTrigger(CONFIG_ADC1_BASE_ADDR, 2, ADC_INT_SOC_TRIGGER_NONE); /* Start of Conversion 3 Configuration */ /* Configures a start-of-conversion (SOC) in the ADC. */ ADC_setupSOC(CONFIG_ADC1_BASE_ADDR, 3, ADC_TRIGGER_SW_ONLY, ADC_CH_ADCIN0, 16); /* Configures the interrupt SOC trigger of an SOC. */ ADC_setInterruptSOCTrigger(CONFIG_ADC1_BASE_ADDR, 3, ADC_INT_SOC_TRIGGER_NONE); /* Start of Conversion 4 Configuration */ /* Configures a start-of-conversion (SOC) in the ADC. */ ADC_setupSOC(CONFIG_ADC1_BASE_ADDR, 4, ADC_TRIGGER_SW_ONLY, ADC_CH_ADCIN0, 16); /* Configures the interrupt SOC trigger of an SOC. */ ADC_setInterruptSOCTrigger(CONFIG_ADC1_BASE_ADDR, 4, ADC_INT_SOC_TRIGGER_NONE); /* Start of Conversion 5 Configuration */ /* Configures a start-of-conversion (SOC) in the ADC. */ ADC_setupSOC(CONFIG_ADC1_BASE_ADDR, 5, ADC_TRIGGER_SW_ONLY, ADC_CH_ADCIN0, 16); /* Configures the interrupt SOC trigger of an SOC. */ ADC_setInterruptSOCTrigger(CONFIG_ADC1_BASE_ADDR, 5, ADC_INT_SOC_TRIGGER_NONE); /* Start of Conversion 6 Configuration */ /* Configures a start-of-conversion (SOC) in the ADC. */ ADC_setupSOC(CONFIG_ADC1_BASE_ADDR, 6, ADC_TRIGGER_SW_ONLY, ADC_CH_ADCIN0, 16); /* Configures the interrupt SOC trigger of an SOC. */ ADC_setInterruptSOCTrigger(CONFIG_ADC1_BASE_ADDR, 6, ADC_INT_SOC_TRIGGER_NONE); /* Start of Conversion 7 Configuration */ /* Configures a start-of-conversion (SOC) in the ADC. */ ADC_setupSOC(CONFIG_ADC1_BASE_ADDR, 7, ADC_TRIGGER_SW_ONLY, ADC_CH_ADCIN0, 16); /* Configures the interrupt SOC trigger of an SOC. */ ADC_setInterruptSOCTrigger(CONFIG_ADC1_BASE_ADDR, 7, ADC_INT_SOC_TRIGGER_NONE); /* Start of Conversion 8 Configuration */ /* Configures a start-of-conversion (SOC) in the ADC. */ ADC_setupSOC(CONFIG_ADC1_BASE_ADDR, 8, ADC_TRIGGER_SW_ONLY, ADC_CH_ADCIN0, 16); /* Configures the interrupt SOC trigger of an SOC. */ ADC_setInterruptSOCTrigger(CONFIG_ADC1_BASE_ADDR, 8, ADC_INT_SOC_TRIGGER_NONE); /* Start of Conversion 9 Configuration */ /* Configures a start-of-conversion (SOC) in the ADC. */ ADC_setupSOC(CONFIG_ADC1_BASE_ADDR, 9, ADC_TRIGGER_SW_ONLY, ADC_CH_ADCIN0, 16); /* Configures the interrupt SOC trigger of an SOC. */ ADC_setInterruptSOCTrigger(CONFIG_ADC1_BASE_ADDR, 9, ADC_INT_SOC_TRIGGER_NONE); /* Start of Conversion 10 Configuration */ /* Configures a start-of-conversion (SOC) in the ADC. */ ADC_setupSOC(CONFIG_ADC1_BASE_ADDR, 10, ADC_TRIGGER_SW_ONLY, ADC_CH_ADCIN0, 16); /* Configures the interrupt SOC trigger of an SOC. */ ADC_setInterruptSOCTrigger(CONFIG_ADC1_BASE_ADDR, 10, ADC_INT_SOC_TRIGGER_NONE); /* Start of Conversion 11 Configuration */ /* Configures a start-of-conversion (SOC) in the ADC. */ ADC_setupSOC(CONFIG_ADC1_BASE_ADDR, 11, ADC_TRIGGER_SW_ONLY, ADC_CH_ADCIN0, 16); /* Configures the interrupt SOC trigger of an SOC. */ ADC_setInterruptSOCTrigger(CONFIG_ADC1_BASE_ADDR, 11, ADC_INT_SOC_TRIGGER_NONE); /* Start of Conversion 12 Configuration */ /* Configures a start-of-conversion (SOC) in the ADC. */ ADC_setupSOC(CONFIG_ADC1_BASE_ADDR, 12, ADC_TRIGGER_SW_ONLY, ADC_CH_ADCIN0, 16); /* Configures the interrupt SOC trigger of an SOC. */ ADC_setInterruptSOCTrigger(CONFIG_ADC1_BASE_ADDR, 12, ADC_INT_SOC_TRIGGER_NONE); /* Start of Conversion 13 Configuration */ /* Configures a start-of-conversion (SOC) in the ADC. */ ADC_setupSOC(CONFIG_ADC1_BASE_ADDR, 13, ADC_TRIGGER_SW_ONLY, ADC_CH_ADCIN0, 16); /* Configures the interrupt SOC trigger of an SOC. */ ADC_setInterruptSOCTrigger(CONFIG_ADC1_BASE_ADDR, 13, ADC_INT_SOC_TRIGGER_NONE); /* Start of Conversion 14 Configuration */ /* Configures a start-of-conversion (SOC) in the ADC. */ ADC_setupSOC(CONFIG_ADC1_BASE_ADDR, 14, ADC_TRIGGER_SW_ONLY, ADC_CH_ADCIN0, 16); /* Configures the interrupt SOC trigger of an SOC. */ ADC_setInterruptSOCTrigger(CONFIG_ADC1_BASE_ADDR, 14, ADC_INT_SOC_TRIGGER_NONE); /* Start of Conversion 15 Configuration */ /* Configures a start-of-conversion (SOC) in the ADC. */ ADC_setupSOC(CONFIG_ADC1_BASE_ADDR, 15, ADC_TRIGGER_SW_ONLY, ADC_CH_ADCIN0, 16); /* Configures the interrupt SOC trigger of an SOC. */ ADC_setInterruptSOCTrigger(CONFIG_ADC1_BASE_ADDR, 15, ADC_INT_SOC_TRIGGER_NONE); /* Powers up the analog-to-digital converter core. */ ADC_enableConverter(CONFIG_ADC1_BASE_ADDR); /* Delay for ADC to power up. */ ClockP_usleep(500); /* Sets the timing of the end-of-conversion pulse */ ADC_setInterruptPulseMode(CONFIG_ADC1_BASE_ADDR, ADC_PULSE_END_OF_ACQ_WIN); /* ADC Interrupt 1 Configuration */ /* Enables an ADC interrupt source. */ ADC_enableInterrupt(CONFIG_ADC1_BASE_ADDR, 0); /* Sets the source EOC for an analog-to-digital converter interrupt. */ ADC_setInterruptSource(CONFIG_ADC1_BASE_ADDR, 0, ADC_SOC_NUMBER0); /* Enables continuous mode for an ADC interrupt. */ ADC_enableContinuousMode(CONFIG_ADC1_BASE_ADDR, 0); /* ADC Interrupt 2 Configuration */ /* Disables an ADC interrupt source. */ ADC_disableInterrupt(CONFIG_ADC1_BASE_ADDR, 1); /* Sets the source EOC for an analog-to-digital converter interrupt. */ ADC_setInterruptSource(CONFIG_ADC1_BASE_ADDR, 1, ADC_SOC_NUMBER0); /* Disables continuous mode for an ADC interrupt. */ ADC_disableContinuousMode(CONFIG_ADC1_BASE_ADDR, 1); /* ADC Interrupt 3 Configuration */ /* Disables an ADC interrupt source. */ ADC_disableInterrupt(CONFIG_ADC1_BASE_ADDR, 2); /* Sets the source EOC for an analog-to-digital converter interrupt. */ ADC_setInterruptSource(CONFIG_ADC1_BASE_ADDR, 2, ADC_SOC_NUMBER0); /* Disables continuous mode for an ADC interrupt. */ ADC_disableContinuousMode(CONFIG_ADC1_BASE_ADDR, 2); /* ADC Interrupt 4 Configuration */ /* Disables an ADC interrupt source. */ ADC_disableInterrupt(CONFIG_ADC1_BASE_ADDR, 3); /* Sets the source EOC for an analog-to-digital converter interrupt. */ ADC_setInterruptSource(CONFIG_ADC1_BASE_ADDR, 3, ADC_SOC_NUMBER0); /* Disables continuous mode for an ADC interrupt. */ ADC_disableContinuousMode(CONFIG_ADC1_BASE_ADDR, 3); /* Post Processing Block 1 Configuration */ /* Configures a post-processing block (PPB) in the ADC. */ ADC_setupPPB(CONFIG_ADC1_BASE_ADDR, 0, ADC_SOC_NUMBER0); /* Disables individual ADC PPB event sources. */ ADC_disablePPBEvent(CONFIG_ADC1_BASE_ADDR, 0, (ADC_EVT_TRIPHI | ADC_EVT_TRIPLO | ADC_EVT_ZERO)); /* Disables individual ADC PPB event interrupt sources. */ ADC_disablePPBEventInterrupt(CONFIG_ADC1_BASE_ADDR, 0, (ADC_EVT_TRIPHI | ADC_EVT_TRIPLO | ADC_EVT_ZERO)); /* Sets the post processing block offset correction. */ ADC_setPPBCalibrationOffset(CONFIG_ADC1_BASE_ADDR, 0, 0); /* Sets the post processing block reference offset. */ ADC_setPPBReferenceOffset(CONFIG_ADC1_BASE_ADDR, 0, 0); /* Disables two's complement capability in the PPB. */ ADC_disablePPBTwosComplement(CONFIG_ADC1_BASE_ADDR, 0); /* Sets the windowed trip limits for a PPB. */ ADC_setPPBTripLimits(CONFIG_ADC1_BASE_ADDR, 0, 0, 0); /* Disables cycle by cycle clear of ADC PPB event flags. */ ADC_disablePPBEventCBCClear(CONFIG_ADC1_BASE_ADDR, 0); /* Post Processing Block 2 Configuration */ /* Configures a post-processing block (PPB) in the ADC. */ ADC_setupPPB(CONFIG_ADC1_BASE_ADDR, 1, ADC_SOC_NUMBER0); /* Disables individual ADC PPB event sources. */ ADC_disablePPBEvent(CONFIG_ADC1_BASE_ADDR, 1, (ADC_EVT_TRIPHI | ADC_EVT_TRIPLO | ADC_EVT_ZERO)); /* Disables individual ADC PPB event interrupt sources. */ ADC_disablePPBEventInterrupt(CONFIG_ADC1_BASE_ADDR, 1, (ADC_EVT_TRIPHI | ADC_EVT_TRIPLO | ADC_EVT_ZERO)); /* Sets the post processing block offset correction. */ ADC_setPPBCalibrationOffset(CONFIG_ADC1_BASE_ADDR, 1, 0); /* Sets the post processing block reference offset. */ ADC_setPPBReferenceOffset(CONFIG_ADC1_BASE_ADDR, 1, 0); /* Disables two's complement capability in the PPB. */ ADC_disablePPBTwosComplement(CONFIG_ADC1_BASE_ADDR, 1); /* Sets the windowed trip limits for a PPB. */ ADC_setPPBTripLimits(CONFIG_ADC1_BASE_ADDR, 1, 0, 0); /* Disables cycle by cycle clear of ADC PPB event flags. */ ADC_disablePPBEventCBCClear(CONFIG_ADC1_BASE_ADDR, 1); /* Post Processing Block 3 Configuration */ /* Configures a post-processing block (PPB) in the ADC. */ ADC_setupPPB(CONFIG_ADC1_BASE_ADDR, 2, ADC_SOC_NUMBER0); /* Disables individual ADC PPB event sources. */ ADC_disablePPBEvent(CONFIG_ADC1_BASE_ADDR, 2, (ADC_EVT_TRIPHI | ADC_EVT_TRIPLO | ADC_EVT_ZERO)); /* Disables individual ADC PPB event interrupt sources. */ ADC_disablePPBEventInterrupt(CONFIG_ADC1_BASE_ADDR, 2, (ADC_EVT_TRIPHI | ADC_EVT_TRIPLO | ADC_EVT_ZERO)); /* Sets the post processing block offset correction. */ ADC_setPPBCalibrationOffset(CONFIG_ADC1_BASE_ADDR, 2, 0); /* Sets the post processing block reference offset. */ ADC_setPPBReferenceOffset(CONFIG_ADC1_BASE_ADDR, 2, 0); /* Disables two's complement capability in the PPB. */ ADC_disablePPBTwosComplement(CONFIG_ADC1_BASE_ADDR, 2); /* Sets the windowed trip limits for a PPB. */ ADC_setPPBTripLimits(CONFIG_ADC1_BASE_ADDR, 2, 0, 0); /* Disables cycle by cycle clear of ADC PPB event flags. */ ADC_disablePPBEventCBCClear(CONFIG_ADC1_BASE_ADDR, 2); /* Post Processing Block 4 Configuration */ /* Configures a post-processing block (PPB) in the ADC. */ ADC_setupPPB(CONFIG_ADC1_BASE_ADDR, 3, ADC_SOC_NUMBER0); /* Disables individual ADC PPB event sources. */ ADC_disablePPBEvent(CONFIG_ADC1_BASE_ADDR, 3, (ADC_EVT_TRIPHI | ADC_EVT_TRIPLO | ADC_EVT_ZERO)); /* Disables individual ADC PPB event interrupt sources. */ ADC_disablePPBEventInterrupt(CONFIG_ADC1_BASE_ADDR, 3, (ADC_EVT_TRIPHI | ADC_EVT_TRIPLO | ADC_EVT_ZERO)); /* Sets the post processing block offset correction. */ ADC_setPPBCalibrationOffset(CONFIG_ADC1_BASE_ADDR, 3, 0); /* Sets the post processing block reference offset. */ ADC_setPPBReferenceOffset(CONFIG_ADC1_BASE_ADDR, 3, 0); /* Disables two's complement capability in the PPB. */ ADC_disablePPBTwosComplement(CONFIG_ADC1_BASE_ADDR, 3); /* Sets the windowed trip limits for a PPB. */ ADC_setPPBTripLimits(CONFIG_ADC1_BASE_ADDR, 3, 0, 0); /* Disables cycle by cycle clear of ADC PPB event flags. */ ADC_disablePPBEventCBCClear(CONFIG_ADC1_BASE_ADDR, 3); /* Set SOC burst mode. */ ADC_setBurstModeConfig(CONFIG_ADC1_BASE_ADDR, ADC_TRIGGER_SW_ONLY, 1); /* Disables SOC burst mode. */ ADC_disableBurstMode(CONFIG_ADC1_BASE_ADDR); } void Drivers_epwmOpen(void) { /* CONFIG_EPWM0 initialization */ /* Time Base */ EPWM_setEmulationMode(CONFIG_EPWM0_BASE_ADDR, EPWM_EMULATION_STOP_AFTER_NEXT_TB); EPWM_setClockPrescaler(CONFIG_EPWM0_BASE_ADDR, EPWM_CLOCK_DIVIDER_1, EPWM_HSCLOCK_DIVIDER_1); EPWM_setTimeBasePeriod(CONFIG_EPWM0_BASE_ADDR, 199); EPWM_disableGlobalLoadRegisters(CONFIG_EPWM0_BASE_ADDR, EPWM_GL_REGISTER_TBPRD_TBPRDHR); EPWM_setPeriodLoadMode(CONFIG_EPWM0_BASE_ADDR, EPWM_PERIOD_SHADOW_LOAD); EPWM_selectPeriodLoadEvent(CONFIG_EPWM0_BASE_ADDR, EPWM_SHADOW_LOAD_MODE_COUNTER_ZERO); EPWM_setTimeBaseCounter(CONFIG_EPWM0_BASE_ADDR, 0); EPWM_setTimeBaseCounterMode(CONFIG_EPWM0_BASE_ADDR, EPWM_COUNTER_MODE_UP); EPWM_setCountModeAfterSync(CONFIG_EPWM0_BASE_ADDR, EPWM_COUNT_MODE_DOWN_AFTER_SYNC); EPWM_disablePhaseShiftLoad(CONFIG_EPWM0_BASE_ADDR); EPWM_setPhaseShift(CONFIG_EPWM0_BASE_ADDR, 0); EPWM_enableSyncOutPulseSource(CONFIG_EPWM0_BASE_ADDR, 0); EPWM_setSyncInPulseSource(CONFIG_EPWM0_BASE_ADDR, EPWM_SYNC_IN_PULSE_SRC_DISABLE); EPWM_setOneShotSyncOutTrigger(CONFIG_EPWM0_BASE_ADDR, EPWM_OSHT_SYNC_OUT_TRIG_SYNC); HRPWM_setSyncPulseSource(CONFIG_EPWM0_BASE_ADDR, HRPWM_PWMSYNC_SOURCE_PERIOD); /* Counter Compare */ EPWM_setCounterCompareValue(CONFIG_EPWM0_BASE_ADDR, EPWM_COUNTER_COMPARE_A, 100); EPWM_disableGlobalLoadRegisters(CONFIG_EPWM0_BASE_ADDR, EPWM_GL_REGISTER_CMPA_CMPAHR); EPWM_setCounterCompareShadowLoadMode(CONFIG_EPWM0_BASE_ADDR, EPWM_COUNTER_COMPARE_A, EPWM_COMP_LOAD_ON_CNTR_ZERO); EPWM_setCounterCompareValue(CONFIG_EPWM0_BASE_ADDR, EPWM_COUNTER_COMPARE_B, 0); EPWM_disableGlobalLoadRegisters(CONFIG_EPWM0_BASE_ADDR, EPWM_GL_REGISTER_CMPB_CMPBHR); EPWM_setCounterCompareShadowLoadMode(CONFIG_EPWM0_BASE_ADDR, EPWM_COUNTER_COMPARE_B, EPWM_COMP_LOAD_ON_CNTR_ZERO); EPWM_setCounterCompareValue(CONFIG_EPWM0_BASE_ADDR, EPWM_COUNTER_COMPARE_C, 0); EPWM_disableGlobalLoadRegisters(CONFIG_EPWM0_BASE_ADDR, EPWM_GL_REGISTER_CMPC); EPWM_setCounterCompareShadowLoadMode(CONFIG_EPWM0_BASE_ADDR, EPWM_COUNTER_COMPARE_C, EPWM_COMP_LOAD_ON_CNTR_ZERO); EPWM_setCounterCompareValue(CONFIG_EPWM0_BASE_ADDR, EPWM_COUNTER_COMPARE_D, 0); EPWM_disableGlobalLoadRegisters(CONFIG_EPWM0_BASE_ADDR, EPWM_GL_REGISTER_CMPD); EPWM_setCounterCompareShadowLoadMode(CONFIG_EPWM0_BASE_ADDR, EPWM_COUNTER_COMPARE_D, EPWM_COMP_LOAD_ON_CNTR_ZERO); /* Action Qualifier */ EPWM_disableGlobalLoadRegisters(CONFIG_EPWM0_BASE_ADDR, EPWM_GL_REGISTER_AQCSFRC); EPWM_setActionQualifierContSWForceShadowMode(CONFIG_EPWM0_BASE_ADDR, EPWM_AQ_SW_SH_LOAD_ON_CNTR_ZERO); EPWM_disableGlobalLoadRegisters(CONFIG_EPWM0_BASE_ADDR, EPWM_GL_REGISTER_AQCTLA_AQCTLA2); EPWM_disableActionQualifierShadowLoadMode(CONFIG_EPWM0_BASE_ADDR, EPWM_ACTION_QUALIFIER_A); EPWM_setActionQualifierShadowLoadMode(CONFIG_EPWM0_BASE_ADDR, EPWM_ACTION_QUALIFIER_A, EPWM_AQ_LOAD_ON_CNTR_ZERO); EPWM_setActionQualifierT1TriggerSource(CONFIG_EPWM0_BASE_ADDR, EPWM_AQ_TRIGGER_EVENT_TRIG_DCA_1); EPWM_setActionQualifierT2TriggerSource(CONFIG_EPWM0_BASE_ADDR, EPWM_AQ_TRIGGER_EVENT_TRIG_DCA_1); EPWM_setActionQualifierSWAction(CONFIG_EPWM0_BASE_ADDR, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_NO_CHANGE); EPWM_setActionQualifierContSWForceAction(CONFIG_EPWM0_BASE_ADDR, EPWM_AQ_OUTPUT_A, EPWM_AQ_SW_DISABLED); EPWM_disableGlobalLoadRegisters(CONFIG_EPWM0_BASE_ADDR, EPWM_GL_REGISTER_AQCTLB_AQCTLB2); EPWM_disableActionQualifierShadowLoadMode(CONFIG_EPWM0_BASE_ADDR, EPWM_ACTION_QUALIFIER_B); EPWM_setActionQualifierShadowLoadMode(CONFIG_EPWM0_BASE_ADDR, EPWM_ACTION_QUALIFIER_B, EPWM_AQ_LOAD_ON_CNTR_ZERO); EPWM_setActionQualifierSWAction(CONFIG_EPWM0_BASE_ADDR, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_NO_CHANGE); EPWM_setActionQualifierContSWForceAction(CONFIG_EPWM0_BASE_ADDR, EPWM_AQ_OUTPUT_B, EPWM_AQ_SW_DISABLED); /* Events */ EPWM_setActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_ZERO); EPWM_setActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_PERIOD); EPWM_setActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPA); EPWM_setActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_DOWN_CMPA); EPWM_setActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPB); EPWM_setActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_DOWN_CMPB); EPWM_setActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_T1_COUNT_UP); EPWM_setActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_T1_COUNT_DOWN); EPWM_setActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_T2_COUNT_UP); EPWM_setActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_T2_COUNT_DOWN); EPWM_setActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_ZERO); EPWM_setActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_PERIOD); EPWM_setActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPA); EPWM_setActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_DOWN_CMPA); EPWM_setActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPB); EPWM_setActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_DOWN_CMPB); EPWM_setActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_T1_COUNT_UP); EPWM_setActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_T1_COUNT_DOWN); EPWM_setActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_T2_COUNT_UP); EPWM_setActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_T2_COUNT_DOWN); /* Trip Zone */ EPWM_setTripZoneAction(CONFIG_EPWM0_BASE_ADDR, EPWM_TZ_ACTION_EVENT_TZA, EPWM_TZ_ACTION_HIGH_Z); EPWM_setTripZoneAction(CONFIG_EPWM0_BASE_ADDR, EPWM_TZ_ACTION_EVENT_TZB, EPWM_TZ_ACTION_HIGH_Z); EPWM_setTripZoneAction(CONFIG_EPWM0_BASE_ADDR, EPWM_TZ_ACTION_EVENT_DCAEVT1, EPWM_TZ_ACTION_HIGH_Z); EPWM_setTripZoneAction(CONFIG_EPWM0_BASE_ADDR, EPWM_TZ_ACTION_EVENT_DCAEVT2, EPWM_TZ_ACTION_HIGH_Z); EPWM_setTripZoneAction(CONFIG_EPWM0_BASE_ADDR, EPWM_TZ_ACTION_EVENT_DCBEVT1, EPWM_TZ_ACTION_HIGH_Z); EPWM_setTripZoneAction(CONFIG_EPWM0_BASE_ADDR, EPWM_TZ_ACTION_EVENT_DCBEVT2, EPWM_TZ_ACTION_HIGH_Z); EPWM_disableTripZoneAdvAction(CONFIG_EPWM0_BASE_ADDR); EPWM_enableTripZoneSignals(CONFIG_EPWM0_BASE_ADDR, 0); EPWM_enableTripZoneSignals(CONFIG_EPWM0_BASE_ADDR, 0); EPWM_selectCycleByCycleTripZoneClearEvent(CONFIG_EPWM0_BASE_ADDR, EPWM_TZ_CBC_PULSE_CLR_CNTR_ZERO); EPWM_enableTripZoneInterrupt(CONFIG_EPWM0_BASE_ADDR, 0); /* Digital Compare */ EPWM_setDigitalCompareFilterInput(CONFIG_EPWM0_BASE_ADDR, EPWM_DC_WINDOW_SOURCE_DCAEVT1); EPWM_disableDigitalCompareBlankingWindow(CONFIG_EPWM0_BASE_ADDR); EPWM_setDigitalCompareBlankingEvent(CONFIG_EPWM0_BASE_ADDR, EPWM_DC_WINDOW_START_TBCTR_PERIOD, 0); EPWM_setDigitalCompareWindowOffset(CONFIG_EPWM0_BASE_ADDR, 0); EPWM_setDigitalCompareWindowLength(CONFIG_EPWM0_BASE_ADDR, 0); EPWM_disableDigitalCompareWindowInverseMode(CONFIG_EPWM0_BASE_ADDR); EPWM_disableDigitalCompareCounterCapture(CONFIG_EPWM0_BASE_ADDR); EPWM_setDigitalCompareCounterShadowMode(CONFIG_EPWM0_BASE_ADDR, false); EPWM_disableDigitalCompareEdgeFilter(CONFIG_EPWM0_BASE_ADDR); EPWM_setDigitalCompareEdgeFilterMode(CONFIG_EPWM0_BASE_ADDR, EPWM_DC_EDGEFILT_MODE_RISING); EPWM_setDigitalCompareEdgeFilterEdgeCount(CONFIG_EPWM0_BASE_ADDR, EPWM_DC_EDGEFILT_EDGECNT_0); EPWM_disableValleyCapture(CONFIG_EPWM0_BASE_ADDR); EPWM_setValleyTriggerSource(CONFIG_EPWM0_BASE_ADDR, EPWM_VALLEY_TRIGGER_EVENT_SOFTWARE); EPWM_setValleyTriggerEdgeCounts(CONFIG_EPWM0_BASE_ADDR, 0, 0); EPWM_disableValleyHWDelay(CONFIG_EPWM0_BASE_ADDR); EPWM_setValleySWDelayValue(CONFIG_EPWM0_BASE_ADDR, 0); EPWM_setValleyDelayDivider(CONFIG_EPWM0_BASE_ADDR, EPWM_VALLEY_DELAY_MODE_SW_DELAY); EPWM_enableDigitalCompareTripCombinationInput(CONFIG_EPWM0_BASE_ADDR, 0, EPWM_DC_TYPE_DCAH); EPWM_selectDigitalCompareTripInput(CONFIG_EPWM0_BASE_ADDR, EPWM_DC_TRIP_TRIPIN1, EPWM_DC_TYPE_DCAH); EPWM_enableDigitalCompareTripCombinationInput(CONFIG_EPWM0_BASE_ADDR, 0, EPWM_DC_TYPE_DCAL); EPWM_selectDigitalCompareTripInput(CONFIG_EPWM0_BASE_ADDR, EPWM_DC_TRIP_TRIPIN1, EPWM_DC_TYPE_DCAL); EPWM_setTripZoneDigitalCompareEventCondition(CONFIG_EPWM0_BASE_ADDR, EPWM_TZ_DC_OUTPUT_A1, EPWM_TZ_EVENT_DC_DISABLED); EPWM_setTripZoneDigitalCompareEventCondition(CONFIG_EPWM0_BASE_ADDR, EPWM_TZ_DC_OUTPUT_A2, EPWM_TZ_EVENT_DC_DISABLED); EPWM_disableDigitalCompareADCTrigger(CONFIG_EPWM0_BASE_ADDR, EPWM_DC_MODULE_A); EPWM_setDigitalCompareEventSyncMode(CONFIG_EPWM0_BASE_ADDR, EPWM_DC_MODULE_A, EPWM_DC_EVENT_1, EPWM_DC_EVENT_INPUT_SYNCED); EPWM_setDigitalCompareEventSource(CONFIG_EPWM0_BASE_ADDR, EPWM_DC_MODULE_A, EPWM_DC_EVENT_1, EPWM_DC_EVENT_SOURCE_ORIG_SIGNAL); EPWM_setDigitalCompareEventSyncMode(CONFIG_EPWM0_BASE_ADDR, EPWM_DC_MODULE_A, EPWM_DC_EVENT_2, EPWM_DC_EVENT_INPUT_SYNCED); EPWM_setDigitalCompareEventSource(CONFIG_EPWM0_BASE_ADDR, EPWM_DC_MODULE_A, EPWM_DC_EVENT_2, EPWM_DC_EVENT_SOURCE_ORIG_SIGNAL); EPWM_enableDigitalCompareTripCombinationInput(CONFIG_EPWM0_BASE_ADDR, 0, EPWM_DC_TYPE_DCBH); EPWM_selectDigitalCompareTripInput(CONFIG_EPWM0_BASE_ADDR, EPWM_DC_TRIP_TRIPIN1, EPWM_DC_TYPE_DCBH); EPWM_enableDigitalCompareTripCombinationInput(CONFIG_EPWM0_BASE_ADDR, 0, EPWM_DC_TYPE_DCBL); EPWM_selectDigitalCompareTripInput(CONFIG_EPWM0_BASE_ADDR, EPWM_DC_TRIP_TRIPIN1, EPWM_DC_TYPE_DCBL); EPWM_setTripZoneDigitalCompareEventCondition(CONFIG_EPWM0_BASE_ADDR, EPWM_TZ_DC_OUTPUT_B1, EPWM_TZ_EVENT_DC_DISABLED); EPWM_setTripZoneDigitalCompareEventCondition(CONFIG_EPWM0_BASE_ADDR, EPWM_TZ_DC_OUTPUT_B2, EPWM_TZ_EVENT_DC_DISABLED); EPWM_disableDigitalCompareADCTrigger(CONFIG_EPWM0_BASE_ADDR, EPWM_DC_MODULE_B); EPWM_setDigitalCompareEventSyncMode(CONFIG_EPWM0_BASE_ADDR, EPWM_DC_MODULE_B, EPWM_DC_EVENT_1, EPWM_DC_EVENT_INPUT_SYNCED); EPWM_setDigitalCompareEventSource(CONFIG_EPWM0_BASE_ADDR, EPWM_DC_MODULE_B, EPWM_DC_EVENT_1, EPWM_DC_EVENT_SOURCE_ORIG_SIGNAL); EPWM_setDigitalCompareEventSyncMode(CONFIG_EPWM0_BASE_ADDR, EPWM_DC_MODULE_B, EPWM_DC_EVENT_2, EPWM_DC_EVENT_INPUT_SYNCED); EPWM_setDigitalCompareEventSource(CONFIG_EPWM0_BASE_ADDR, EPWM_DC_MODULE_B, EPWM_DC_EVENT_2, EPWM_DC_EVENT_SOURCE_ORIG_SIGNAL); EPWM_setDigitalCompareCBCLatchMode(CONFIG_EPWM0_BASE_ADDR, EPWM_DC_MODULE_A, EPWM_DC_EVENT_1, EPWM_DC_CBC_LATCH_DISABLED); EPWM_selectDigitalCompareCBCLatchClearEvent(CONFIG_EPWM0_BASE_ADDR, EPWM_DC_MODULE_A, EPWM_DC_EVENT_1, EPWM_DC_CBC_LATCH_CLR_CNTR_ZERO); EPWM_setDigitalCompareCBCLatchMode(CONFIG_EPWM0_BASE_ADDR, EPWM_DC_MODULE_A, EPWM_DC_EVENT_2, EPWM_DC_CBC_LATCH_DISABLED); EPWM_selectDigitalCompareCBCLatchClearEvent(CONFIG_EPWM0_BASE_ADDR, EPWM_DC_MODULE_A, EPWM_DC_EVENT_2, EPWM_DC_CBC_LATCH_CLR_CNTR_ZERO); EPWM_setDigitalCompareCBCLatchMode(CONFIG_EPWM0_BASE_ADDR, EPWM_DC_MODULE_B, EPWM_DC_EVENT_1, EPWM_DC_CBC_LATCH_DISABLED); EPWM_selectDigitalCompareCBCLatchClearEvent(CONFIG_EPWM0_BASE_ADDR, EPWM_DC_MODULE_B, EPWM_DC_EVENT_1, EPWM_DC_CBC_LATCH_CLR_CNTR_ZERO); EPWM_setDigitalCompareCBCLatchMode(CONFIG_EPWM0_BASE_ADDR, EPWM_DC_MODULE_B, EPWM_DC_EVENT_2, EPWM_DC_CBC_LATCH_DISABLED); EPWM_selectDigitalCompareCBCLatchClearEvent(CONFIG_EPWM0_BASE_ADDR, EPWM_DC_MODULE_B, EPWM_DC_EVENT_2, EPWM_DC_CBC_LATCH_CLR_CNTR_ZERO); /* Deadband */ EPWM_disableDeadBandControlShadowLoadMode(CONFIG_EPWM0_BASE_ADDR); EPWM_setDeadBandControlShadowLoadMode(CONFIG_EPWM0_BASE_ADDR, EPWM_DB_LOAD_ON_CNTR_ZERO); EPWM_setRisingEdgeDeadBandDelayInput(CONFIG_EPWM0_BASE_ADDR, EPWM_DB_INPUT_EPWMA); EPWM_setFallingEdgeDeadBandDelayInput(CONFIG_EPWM0_BASE_ADDR, EPWM_DB_INPUT_EPWMA); EPWM_setDeadBandDelayPolarity(CONFIG_EPWM0_BASE_ADDR, EPWM_DB_RED, EPWM_DB_POLARITY_ACTIVE_HIGH); EPWM_setDeadBandDelayPolarity(CONFIG_EPWM0_BASE_ADDR, EPWM_DB_FED, EPWM_DB_POLARITY_ACTIVE_HIGH); EPWM_setDeadBandDelayMode(CONFIG_EPWM0_BASE_ADDR, EPWM_DB_RED, false); EPWM_setDeadBandDelayMode(CONFIG_EPWM0_BASE_ADDR, EPWM_DB_FED, false); EPWM_setDeadBandOutputSwapMode(CONFIG_EPWM0_BASE_ADDR, EPWM_DB_OUTPUT_A, false); EPWM_setDeadBandOutputSwapMode(CONFIG_EPWM0_BASE_ADDR, EPWM_DB_OUTPUT_B, false); EPWM_disableRisingEdgeDelayCountShadowLoadMode(CONFIG_EPWM0_BASE_ADDR); EPWM_setRisingEdgeDelayCountShadowLoadMode(CONFIG_EPWM0_BASE_ADDR, EPWM_RED_LOAD_ON_CNTR_ZERO); EPWM_setRisingEdgeDelayCount(CONFIG_EPWM0_BASE_ADDR, 0); EPWM_disableFallingEdgeDelayCountShadowLoadMode(CONFIG_EPWM0_BASE_ADDR); EPWM_setFallingEdgeDelayCountShadowLoadMode(CONFIG_EPWM0_BASE_ADDR, EPWM_FED_LOAD_ON_CNTR_ZERO); EPWM_setFallingEdgeDelayCount(CONFIG_EPWM0_BASE_ADDR, 0); EPWM_setDeadBandCounterClock(CONFIG_EPWM0_BASE_ADDR, EPWM_DB_COUNTER_CLOCK_FULL_CYCLE); /* Chopper */ EPWM_disableChopper(CONFIG_EPWM0_BASE_ADDR); EPWM_setChopperDutyCycle(CONFIG_EPWM0_BASE_ADDR, 0); EPWM_setChopperFreq(CONFIG_EPWM0_BASE_ADDR, 0); EPWM_setChopperFirstPulseWidth(CONFIG_EPWM0_BASE_ADDR, 0); /* Event Trigger */ EPWM_disableInterrupt(CONFIG_EPWM0_BASE_ADDR); EPWM_setInterruptSource(CONFIG_EPWM0_BASE_ADDR, EPWM_INT_TBCTR_ZERO, 0); EPWM_setInterruptEventCount(CONFIG_EPWM0_BASE_ADDR, 0); EPWM_disableInterruptEventCountInit(CONFIG_EPWM0_BASE_ADDR); EPWM_setInterruptEventCountInitValue(CONFIG_EPWM0_BASE_ADDR, 0); EPWM_enableADCTrigger(CONFIG_EPWM0_BASE_ADDR, EPWM_SOC_A); EPWM_setADCTriggerSource(CONFIG_EPWM0_BASE_ADDR, EPWM_SOC_A, EPWM_SOC_TBCTR_ZERO, 0); EPWM_setADCTriggerEventPrescale(CONFIG_EPWM0_BASE_ADDR, EPWM_SOC_A, 1); EPWM_enableADCTriggerEventCountInit(CONFIG_EPWM0_BASE_ADDR, EPWM_SOC_A); EPWM_setADCTriggerEventCountInitValue(CONFIG_EPWM0_BASE_ADDR, EPWM_SOC_A, 0); EPWM_disableADCTrigger(CONFIG_EPWM0_BASE_ADDR, EPWM_SOC_B); EPWM_setADCTriggerSource(CONFIG_EPWM0_BASE_ADDR, EPWM_SOC_B, EPWM_SOC_DCxEVT1, EPWM_SOC_DCxEVT1); EPWM_setADCTriggerEventPrescale(CONFIG_EPWM0_BASE_ADDR, EPWM_SOC_B, 0); EPWM_disableADCTriggerEventCountInit(CONFIG_EPWM0_BASE_ADDR, EPWM_SOC_B); EPWM_setADCTriggerEventCountInitValue(CONFIG_EPWM0_BASE_ADDR, EPWM_SOC_B, 0); /* XCMP Mode */ EPWM_disableXCMPMode(CONFIG_EPWM0_BASE_ADDR); EPWM_disableSplitXCMP(CONFIG_EPWM0_BASE_ADDR); EPWM_allocAXCMP(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP_NONE_CMPA); EPWM_setXCMPLoadMode(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP_XLOADCTL_LOADMODE_LOADONCE); EPWM_setXCMPShadowLevel(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP_XLOADCTL_SHDWLEVEL_0); EPWM_setXCMPShadowBufPtrLoadOnce(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP_XLOADCTL_SHDWBUFPTR_NULL); EPWM_setXCMPShadowRepeatBufxCount(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP_SHADOW2, 0); EPWM_setXCMPShadowRepeatBufxCount(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP_SHADOW3, 0); /* Write values to Reg */ EPWM_setXCMPRegValue(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP1_ACTIVE, 0); EPWM_setXCMPRegValue(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP2_ACTIVE, 0); EPWM_setXCMPRegValue(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP3_ACTIVE, 0); EPWM_setXCMPRegValue(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP4_ACTIVE, 0); EPWM_setXCMPRegValue(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP5_ACTIVE, 0); EPWM_setXCMPRegValue(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP6_ACTIVE, 0); EPWM_setXCMPRegValue(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP7_ACTIVE, 0); EPWM_setXCMPRegValue(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP8_ACTIVE, 0); EPWM_setXCMPRegValue(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP1_SHADOW1, 0); EPWM_setXCMPRegValue(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP2_SHADOW1, 0); EPWM_setXCMPRegValue(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP3_SHADOW1, 0); EPWM_setXCMPRegValue(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP4_SHADOW1, 0); EPWM_setXCMPRegValue(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP5_SHADOW1, 0); EPWM_setXCMPRegValue(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP6_SHADOW1, 0); EPWM_setXCMPRegValue(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP7_SHADOW1, 0); EPWM_setXCMPRegValue(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP8_SHADOW1, 0); EPWM_setXCMPRegValue(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP1_SHADOW2, 0); EPWM_setXCMPRegValue(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP2_SHADOW2, 0); EPWM_setXCMPRegValue(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP3_SHADOW2, 0); EPWM_setXCMPRegValue(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP4_SHADOW2, 0); EPWM_setXCMPRegValue(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP5_SHADOW2, 0); EPWM_setXCMPRegValue(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP6_SHADOW2, 0); EPWM_setXCMPRegValue(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP7_SHADOW2, 0); EPWM_setXCMPRegValue(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP8_SHADOW2, 0); EPWM_setXCMPRegValue(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP1_SHADOW3, 0); EPWM_setXCMPRegValue(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP2_SHADOW3, 0); EPWM_setXCMPRegValue(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP3_SHADOW3, 0); EPWM_setXCMPRegValue(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP4_SHADOW3, 0); EPWM_setXCMPRegValue(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP5_SHADOW3, 0); EPWM_setXCMPRegValue(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP6_SHADOW3, 0); EPWM_setXCMPRegValue(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP7_SHADOW3, 0); EPWM_setXCMPRegValue(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP8_SHADOW3, 0); EPWM_setXCMPRegValue(CONFIG_EPWM0_BASE_ADDR, EPWM_XTBPRD_ACTIVE, 0); EPWM_setXCMPRegValue(CONFIG_EPWM0_BASE_ADDR, EPWM_XTBPRD_SHADOW1, 0); EPWM_setXCMPRegValue(CONFIG_EPWM0_BASE_ADDR, EPWM_XTBPRD_SHADOW2, 0); EPWM_setXCMPRegValue(CONFIG_EPWM0_BASE_ADDR, EPWM_XTBPRD_SHADOW3, 0); EPWM_setXMINMAXRegValue(CONFIG_EPWM0_BASE_ADDR, EPWM_XMIN_ACTIVE, 0); EPWM_setXMINMAXRegValue(CONFIG_EPWM0_BASE_ADDR, EPWM_XMAX_ACTIVE, 0); EPWM_setXMINMAXRegValue(CONFIG_EPWM0_BASE_ADDR, EPWM_XMIN_SHADOW1, 0); EPWM_setXMINMAXRegValue(CONFIG_EPWM0_BASE_ADDR, EPWM_XMAX_SHADOW1, 0); EPWM_setXMINMAXRegValue(CONFIG_EPWM0_BASE_ADDR, EPWM_XMIN_SHADOW2, 0); EPWM_setXMINMAXRegValue(CONFIG_EPWM0_BASE_ADDR, EPWM_XMAX_SHADOW2, 0); EPWM_setXMINMAXRegValue(CONFIG_EPWM0_BASE_ADDR, EPWM_XMIN_SHADOW3, 0); EPWM_setXMINMAXRegValue(CONFIG_EPWM0_BASE_ADDR, EPWM_XMAX_SHADOW3, 0); /* Events */ EPWM_setXCMPActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP_ACTIVE, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_XCMP1); EPWM_setXCMPActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP_ACTIVE, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_XCMP2); EPWM_setXCMPActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP_ACTIVE, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_XCMP3); EPWM_setXCMPActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP_ACTIVE, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_XCMP4); EPWM_setXCMPActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP_ACTIVE, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_XCMP5); EPWM_setXCMPActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP_ACTIVE, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_XCMP6); EPWM_setXCMPActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP_ACTIVE, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_XCMP7); EPWM_setXCMPActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP_ACTIVE, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_XCMP8); EPWM_setXCMPActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP_ACTIVE, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_XCMP5); EPWM_setXCMPActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP_ACTIVE, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_XCMP6); EPWM_setXCMPActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP_ACTIVE, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_XCMP7); EPWM_setXCMPActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP_ACTIVE, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_XCMP8); EPWM_setXCMPActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP_SHADOW1, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_XCMP1); EPWM_setXCMPActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP_SHADOW1, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_XCMP2); EPWM_setXCMPActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP_SHADOW1, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_XCMP3); EPWM_setXCMPActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP_SHADOW1, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_XCMP4); EPWM_setXCMPActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP_SHADOW1, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_XCMP5); EPWM_setXCMPActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP_SHADOW1, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_XCMP6); EPWM_setXCMPActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP_SHADOW1, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_XCMP7); EPWM_setXCMPActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP_SHADOW1, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_XCMP8); EPWM_setXCMPActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP_SHADOW1, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_XCMP5); EPWM_setXCMPActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP_SHADOW1, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_XCMP6); EPWM_setXCMPActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP_SHADOW1, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_XCMP7); EPWM_setXCMPActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP_SHADOW1, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_XCMP8); EPWM_setXCMPActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP_SHADOW2, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_XCMP1); EPWM_setXCMPActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP_SHADOW2, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_XCMP2); EPWM_setXCMPActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP_SHADOW2, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_XCMP3); EPWM_setXCMPActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP_SHADOW2, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_XCMP4); EPWM_setXCMPActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP_SHADOW2, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_XCMP5); EPWM_setXCMPActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP_SHADOW2, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_XCMP6); EPWM_setXCMPActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP_SHADOW2, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_XCMP7); EPWM_setXCMPActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP_SHADOW2, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_XCMP8); EPWM_setXCMPActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP_SHADOW2, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_XCMP5); EPWM_setXCMPActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP_SHADOW2, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_XCMP6); EPWM_setXCMPActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP_SHADOW2, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_XCMP7); EPWM_setXCMPActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP_SHADOW2, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_XCMP8); EPWM_setXCMPActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP_SHADOW3, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_XCMP1); EPWM_setXCMPActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP_SHADOW3, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_XCMP2); EPWM_setXCMPActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP_SHADOW3, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_XCMP3); EPWM_setXCMPActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP_SHADOW3, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_XCMP4); EPWM_setXCMPActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP_SHADOW3, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_XCMP5); EPWM_setXCMPActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP_SHADOW3, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_XCMP6); EPWM_setXCMPActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP_SHADOW3, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_XCMP7); EPWM_setXCMPActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP_SHADOW3, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_XCMP8); EPWM_setXCMPActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP_SHADOW3, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_XCMP5); EPWM_setXCMPActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP_SHADOW3, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_XCMP6); EPWM_setXCMPActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP_SHADOW3, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_XCMP7); EPWM_setXCMPActionQualifierAction(CONFIG_EPWM0_BASE_ADDR, EPWM_XCMP_SHADOW3, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_NO_CHANGE, EPWM_AQ_OUTPUT_ON_TIMEBASE_XCMP8); /* Diode Emulation */ EPWM_disableDiodeEmulationMode(CONFIG_EPWM0_BASE_ADDR); EPWM_setDiodeEmulationMode(CONFIG_EPWM0_BASE_ADDR, EPWM_DIODE_EMULATION_CBC); EPWM_setDiodeEmulationReentryDelay(CONFIG_EPWM0_BASE_ADDR, 0); EPWM_configureDiodeEmulationTripSources(CONFIG_EPWM0_BASE_ADDR, EPWM_DE_TRIP_SRC_INPUTXBAR_OUT0, EPWM_DE_TRIPL); EPWM_configureDiodeEmulationTripSources(CONFIG_EPWM0_BASE_ADDR, EPWM_DE_TRIP_SRC_INPUTXBAR_OUT0, EPWM_DE_TRIPH); EPWM_selectDiodeEmulationPWMsignal(CONFIG_EPWM0_BASE_ADDR, EPWM_DE_CHANNEL_A, EPWM_DE_SYNC_TRIPHorL); EPWM_selectDiodeEmulationTripSignal(CONFIG_EPWM0_BASE_ADDR, EPWM_DE_CHANNEL_A, EPWM_DE_TRIPL); EPWM_selectDiodeEmulationPWMsignal(CONFIG_EPWM0_BASE_ADDR, EPWM_DE_CHANNEL_B, EPWM_DE_SYNC_TRIPHorL); EPWM_selectDiodeEmulationTripSignal(CONFIG_EPWM0_BASE_ADDR, EPWM_DE_CHANNEL_B, EPWM_DE_TRIPL); EPWM_nobypassDiodeEmulationLogic(CONFIG_EPWM0_BASE_ADDR); EPWM_disableDiodeEmulationMonitorModeControl(CONFIG_EPWM0_BASE_ADDR); EPWM_setDiodeEmulationMonitorCounterThreshold(CONFIG_EPWM0_BASE_ADDR, 0); EPWM_setDiodeEmulationMonitorModeStep(CONFIG_EPWM0_BASE_ADDR, EPWM_DE_COUNT_DOWN, 0); EPWM_setDiodeEmulationMonitorModeStep(CONFIG_EPWM0_BASE_ADDR, EPWM_DE_COUNT_UP, 0); /* HRPWM */ HRPWM_disableAutoConversion(CONFIG_EPWM0_BASE_ADDR); HRPWM_setMEPControlMode(CONFIG_EPWM0_BASE_ADDR, HRPWM_CHANNEL_A, HRPWM_MEP_DUTY_PERIOD_CTRL); HRPWM_setMEPControlMode(CONFIG_EPWM0_BASE_ADDR, HRPWM_CHANNEL_B, HRPWM_MEP_DUTY_PERIOD_CTRL); HRPWM_setHiResPhaseShift(CONFIG_EPWM0_BASE_ADDR, 0); HRPWM_disablePhaseShiftLoad(CONFIG_EPWM0_BASE_ADDR); HRPWM_setMEPEdgeSelect(CONFIG_EPWM0_BASE_ADDR, HRPWM_CHANNEL_A, HRPWM_MEP_CTRL_DISABLE); HRPWM_setMEPEdgeSelect(CONFIG_EPWM0_BASE_ADDR, HRPWM_CHANNEL_B, HRPWM_MEP_CTRL_DISABLE); HRPWM_setHiResCounterCompareValue(CONFIG_EPWM0_BASE_ADDR, HRPWM_COUNTER_COMPARE_A, 1); HRPWM_setHiResCounterCompareValue(CONFIG_EPWM0_BASE_ADDR, HRPWM_COUNTER_COMPARE_B, 1); HRPWM_setCounterCompareShadowLoadEvent(CONFIG_EPWM0_BASE_ADDR, HRPWM_CHANNEL_A, HRPWM_LOAD_ON_CNTR_ZERO); HRPWM_setCounterCompareShadowLoadEvent(CONFIG_EPWM0_BASE_ADDR, HRPWM_CHANNEL_B, HRPWM_LOAD_ON_CNTR_ZERO); HRPWM_disablePeriodControl(CONFIG_EPWM0_BASE_ADDR); HRPWM_setHiResTimeBasePeriod(CONFIG_EPWM0_BASE_ADDR, 0); HRPWM_setDeadbandMEPEdgeSelect(CONFIG_EPWM0_BASE_ADDR, HRPWM_DB_MEP_CTRL_DISABLE); HRPWM_setHiResRisingEdgeDelay(CONFIG_EPWM0_BASE_ADDR, 0); HRPWM_setRisingEdgeDelayLoadMode(CONFIG_EPWM0_BASE_ADDR, HRPWM_LOAD_ON_CNTR_ZERO); HRPWM_setHiResFallingEdgeDelayOnly(CONFIG_EPWM0_BASE_ADDR, 0); HRPWM_setFallingEdgeDelayLoadMode(CONFIG_EPWM0_BASE_ADDR, HRPWM_LOAD_ON_CNTR_ZERO); HRPWM_setOutputSwapMode(CONFIG_EPWM0_BASE_ADDR, false); HRPWM_setChannelBOutputPath(CONFIG_EPWM0_BASE_ADDR, HRPWM_OUTPUT_ON_B_NORMAL); /* ICL */ EPWM_disableIllegalComboLogic(CONFIG_EPWM0_BASE_ADDR, EPWM_MINDB_BLOCK_A); EPWM_disableIllegalComboLogic(CONFIG_EPWM0_BASE_ADDR, EPWM_MINDB_BLOCK_B); /* MDL */ EPWM_disableMinimumDeadBand(CONFIG_EPWM0_BASE_ADDR, EPWM_MINDB_BLOCK_A); EPWM_disableMinimumDeadBand(CONFIG_EPWM0_BASE_ADDR, EPWM_MINDB_BLOCK_B); /* Global Load */ EPWM_disableGlobalLoad(CONFIG_EPWM0_BASE_ADDR); EPWM_setGlobalLoadTrigger(CONFIG_EPWM0_BASE_ADDR, EPWM_GL_LOAD_PULSE_CNTR_ZERO); EPWM_setGlobalLoadEventPrescale(CONFIG_EPWM0_BASE_ADDR, 0); EPWM_disableGlobalLoadOneShotMode(CONFIG_EPWM0_BASE_ADDR); /* EPWM Module */ EPWM_lockRegisters(CONFIG_EPWM0_BASE_ADDR, 0); } void Drivers_intXbarOpen() { /* INT XBAR */ SOC_xbarSelectInterruptXBarInputSource(CSL_CONTROLSS_INTXBAR_U_BASE, 0, 0, 0, ( INT_XBAR_ADC1_INT1 ), 0, 0, 0, 0); } /* * UART */ /* UART Driver handles */ UART_Handle gUartHandle[CONFIG_UART_NUM_INSTANCES]; #include <drivers/uart/v0/lld/dma/uart_dma.h> #include <kernel/dpl/ClockP.h> #include <drivers/edma.h> /* EDMA driver confiurations */ EDMA_Config gEdmaConfig[] = { }; uint32_t gEdmaConfigNum = 0; UART_DmaChConfig gUartDmaChConfig[CONFIG_UART_NUM_INSTANCES] = { NULL, }; /* UART Driver Parameters */ UART_Params gUartParams[CONFIG_UART_NUM_INSTANCES] = { { .baudRate = 115200, .dataLength = UART_LEN_8, .stopBits = UART_STOPBITS_1, .parityType = UART_PARITY_NONE, .readMode = UART_TRANSFER_MODE_BLOCKING, .readReturnMode = UART_READ_RETURN_MODE_FULL, .writeMode = UART_TRANSFER_MODE_BLOCKING, .readCallbackFxn = NULL, .writeCallbackFxn = NULL, .hwFlowControl = FALSE, .hwFlowControlThr = UART_RXTRIGLVL_16, .transferMode = UART_CONFIG_MODE_INTERRUPT, .skipIntrReg = FALSE, .uartDmaIndex = -1, .intrNum = 38U, .intrPriority = 4U, .operMode = UART_OPER_MODE_16X, .rxTrigLvl = UART_RXTRIGLVL_8, .txTrigLvl = UART_TXTRIGLVL_32, .rxEvtNum = 0U, .txEvtNum = 0U, }, }; void Drivers_uartOpen(void) { uint32_t instCnt; int32_t status = SystemP_SUCCESS; for(instCnt = 0U; instCnt < CONFIG_UART_NUM_INSTANCES; instCnt++) { gUartHandle[instCnt] = NULL; /* Init to NULL so that we can exit gracefully */ } /* Open all instances */ for(instCnt = 0U; instCnt < CONFIG_UART_NUM_INSTANCES; instCnt++) { gUartHandle[instCnt] = UART_open(instCnt, &gUartParams[instCnt]); if(NULL == gUartHandle[instCnt]) { DebugP_logError("UART open failed for instance %d !!!\r\n", instCnt); status = SystemP_FAILURE; break; } } if(SystemP_FAILURE == status) { Drivers_uartClose(); /* Exit gracefully */ } return; } void Drivers_uartClose(void) { uint32_t instCnt; /* Close all instances that are open */ for(instCnt = 0U; instCnt < CONFIG_UART_NUM_INSTANCES; instCnt++) { if(gUartHandle[instCnt] != NULL) { UART_close(gUartHandle[instCnt]); gUartHandle[instCnt] = NULL; } } return; }
/* * Copyright (C) 2022-2023 Texas Instruments Incorporated * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the * distribution. * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. */ #include <stdio.h> #include <kernel/dpl/DebugP.h> #include <kernel/dpl/ClockP.h> #include <kernel/dpl/HwiP.h> #include <drivers/epwm.h> #include <drivers/adc.h> #include "ti_drivers_config.h" #include "ti_drivers_open_close.h" #include "ti_board_open_close.h" /* * Example Description : * This examples demonstrates periodical triggering of conversion on ADC1 * by EPWM0 * * SOC Configurations : * - SOC 0 trigger is set by EPWM0SOCA * - Samples on ADC1 Channel 0 * * Interrupt Configurations : * - ADC1INT1 source is set to EOC/SOC0 * - INTXBAR0 is set to ADC1INT1. * * ISR App_adcISR * - reads the SOC0 result. * * External Connections : * - CC: * feed analog input on ADC 1 Channel 0 - HSEC connecter pin - 12 * - LP: * feed analog input on ADC 1 Channel 0 - J1/J3 Pin - 24 * * Watch Variables : * - gAdc1Result0 : the array holds the sampled values of the ADC 1 Channel 0 */ /* Number of ADC conversions required */ #define ADC_CONVERSION_COUNT 400 /* Global variables and objects */ volatile uint32_t gAdc1Result0[ADC_CONVERSION_COUNT]; volatile uint32_t gIndex = 0; uint32_t gAdc1baseAddr = CONFIG_ADC1_BASE_ADDR; uint32_t gAdc1resultBaseAddr = CONFIG_ADC1_RESULT_BASE_ADDR; static HwiP_Object gAdcHwiObject; /* Variable to store the count of completed conversions Initialising conversion count to 0 */ volatile uint32_t gAdcConversionCount = 0; static void App_adcISR(void *args); void adc_soc_epwm_main(void *args) { /* Open drivers to open the UART driver for console */ Drivers_open(); Board_driversOpen(); DebugP_log("ADC Soc EPWM Test Started\r\n"); int32_t status; /* Initialising a Interrupt parameter */ HwiP_Params hwiPrms; /* Register & enable interrupt */ HwiP_Params_init(&hwiPrms); hwiPrms.intNum = CSLR_R5FSS0_CORE0_CONTROLSS_INTRXBAR0_OUT_0; hwiPrms.priority = 0; /* setting high priority. optional */ hwiPrms.callback = &App_adcISR; status = HwiP_construct(&gAdcHwiObject, &hwiPrms); DebugP_assert(status == SystemP_SUCCESS); /* Starting the EPWM-TB Counter*/ EPWM_setTimeBaseCounterMode(CONFIG_EPWM0_BASE_ADDR, EPWM_COUNTER_MODE_UP); /* Wait until all the conversions are done.*/ while (gAdcConversionCount < ADC_CONVERSION_COUNT); DebugP_log("ADC1 SOC0 results\r\n"); for(int iter = 0; iter < gIndex; iter+= 1) { DebugP_log("\t%d\r\n",gAdc1Result0[iter]); } DebugP_log("ADC Soc EPWM Test Passed\r\n"); DebugP_log("All tests have passed!!\r\n"); Board_driversClose(); Drivers_close(); } static void App_adcISR(void *args) { // printf("inside the printf \n"); if (gAdcConversionCount < ADC_CONVERSION_COUNT) { ADC_clearInterruptStatus(gAdc1baseAddr, ADC_INT_NUMBER1); gAdc1Result0[gIndex] = ADC_readResult(gAdc1resultBaseAddr, ADC_SOC_NUMBER0); gIndex++; gAdcConversionCount++; // printf("%d \n",gAdc1Result0[gIndex]); } else { /* stopping the TBCounter to halt PWM*/ EPWM_setTimeBaseCounterMode(CONFIG_EPWM0_BASE_ADDR, EPWM_COUNTER_MODE_STOP_FREEZE); } ADC_clearInterruptStatus(gAdc1baseAddr, ADC_INT_NUMBER1); if(true == ADC_getInterruptOverflowStatus(gAdc1baseAddr, ADC_INT_NUMBER1)) { ADC_clearInterruptStatus(gAdc1baseAddr, ADC_INT_NUMBER1); ADC_clearInterruptOverflowStatus(gAdc1baseAddr, ADC_INT_NUMBER1); } }
pls tell where i am getting wrong?
Hello Tej_1441,
Is it possible to insert some kind of voltage buffer on the input? Can you share the specs of the signal generator you are using? I don't see any issue with your code, but believe the issue could be related to the drive strength of your instrument.
Best Regards,
Zackary Fleenor
Hii Fleenor,
It is not possible to insert voltage buffer.
I am using Tektronix signal generator with model number AFG31000 SERIES Arbitrary function generator.
https://www.tek.com/en/datasheet/arbitrary-function-generators
Here i have attached the image of plotted graph for constant amplitude( amplitude = 0.5v and offset = 0.250v) and different frequency for ADC conversion.
Sampling rate is set to 4MSPS and frequency for triggering SOC from epwm is set to be 1MHz.
why on increasing frequency, range of value captured by ADC is decreasing.
And i am receiving 50 sample at 20KHz which means sampling rate=1msps ( Is sampling rate effected by frequency by which we trigger adc SOC)
graph at 5KHz
graph at 10 KHz
graph at 20 KHz
graph at 50KHz
Graph at 100KHz
Graph at 200KHz
graph at 400KHz
Hey Tej_1441,
I spoke with the design engineer here and came up with the following feedback.
1) It looks like a low-pass filter in the HW is acting upon the signal. Can you check the board for any possible LPF elements?
2) If the EPWM SoC Trigger is set to 1MHz, then you are only generating data at 1MSPS. (The EPWM trigger rate is directly related to the sampling rate).
3) Can you also please provide captures of the input waveform? The "InstaView" technology of the Function Generator you are using seems promising to provide some additional clues.
Best Regards,
Zackary Fleenor
Hii Fleenor,
I am using sitara AM263x MCU with PART NO : LP-AM263.
1 ) I have checked the HW, but there is no LPF elements.
2 ) It can be noticed from the images in previous reply that number of sample for 1MHz is correct ( trigger for ADC's SOC is set to 1MHz), But the problem is that signal is not getting uniformly sampled.
Here i am attaching the captures of input waveform
Here are details obtained from the "InstaView" technology of Function Generator.
DHCP On CLOCK_REFERENCE Internal GPIB_ADDRESS 1.10000000000000000000e+01 GPIB_CONFIGURATION Talk/Listen LANGUAGE English SCREEN_SAVER Off CONTRAST 7.00000000000000000000e+01 CLICK_TONE On SOFT_KEYBOARD On BEEPER On POWER_ON Default BRIGHTNESS 1.00000000000000000000e+02 TRIGGER_SOURCE External TRIGGER_SLOPE Positive TRIGGER_INTERVAL 1.00000000000000002082e-03 TRIGGER_OUT Trigger TIMEZONE UTC+08:00 USB_ESER 0.00000000000000000000e+00 USB_SRER 0.00000000000000000000e+00 USB_QEN 0.00000000000000000000e+00 USB_OEN 0.00000000000000000000e+00 USB_PSC On GPIB_ESER 0.00000000000000000000e+00 GPIB_SRER 0.00000000000000000000e+00 GPIB_QEN 0.00000000000000000000e+00 GPIB_OEN 0.00000000000000000000e+00 GPIB_PSC On VXI11_ESER 0.00000000000000000000e+00 VXI11_SRER 0.00000000000000000000e+00 VXI11_QEN 0.00000000000000000000e+00 VXI11_OEN 0.00000000000000000000e+00 VXI11_PSC On BURST_COUNT1 5.00000000000000000000e+00 BURST_MODE1 Triggered FREQUENCY_CONCURRENT1 Off FUNCTION1 Sine FUNCTION_FILE1 "" VOLTAGE_CONCURRENT1 Off LOAD_IMPEDANCE1 5.00000000000000000000e+01 AMPLITUDE_UNIT1 Vpp AMPLITUDE_VPP1 5.00000000000000000000e-01 AMPLITUDE_VRMS1 1.76776695296636865429e-01 AMPLITUDE_DBM1 -2.04119982655924836479e+00 OFFSET1 2.50000000000000000000e-01 HIGH_LEVEL1 5.00000000000000000000e-01 LOW_LEVEL1 0.00000000000000000000e+00 AMPLITUDE_OR_LEVEL1 Amplitude HIGH_LIMIT1 2.50000000000000000000e+00 LOW_LIMIT1 -2.50000000000000000000e+00 INVERT1 Off NOISE_ADD1 Off NOISE_LEVEL1 1.00000000000000000000e+01 EXTERNAL_ADD1 Off PULSE_WIDTH1 5.00000000000000040902e-06 PULSE_DUTY1 5.00000000000000000000e+01 PULSE_WIDTH_OR_DUTY1 Duty PULSE_LEADING_EDGE1 2.00000000000000012456e-09 PULSE_TRAILING_EDGE1 2.00000000000000012456e-09 RAMP_SYMMETRY1 5.00000000000000000000e+01 NOISE_SIGMA1 2.00000000000000011102e-01 FREQUENCY1 1.00000000000000000000e+05 PERIOD1 1.00000000000000008180e-05 FREQUENCY_OR_PERIOD1 Frequency PHASE1 0.00000000000000000000e+00 LEAD_DELAY1 0.00000000000000000000e+00 PHASE_CONCURRENT1 Off RUN_MODE1 Continuous MODULATION_TYPE1 AM AM_SOURCE1 Internal AM_SHAPE1 Sine AM_SHAPE_FILE1 "" AM_FREQUENCY1 1.00000000000000000000e+04 AM_DEPTH1 5.00000000000000000000e+01 FM_SOURCE1 Internal FM_SHAPE1 Sine FM_SHAPE_FILE1 "" FM_FREQUENCY1 1.00000000000000000000e+04 FM_DEVIATION1 1.00000000000000000000e+06 PM_SOURCE1 Internal PM_SHAPE1 Sine PM_SHAPE_FILE1 "" PM_FREQUENCY1 1.00000000000000000000e+04 PM_DEVIATION1 9.00000000000000000000e+01 PWM_SOURCE1 Internal PWM_SHAPE1 Sine PWM_SHAPE_FILE1 "" PWM_FREQUENCY1 1.00000000000000000000e+04 PWM_DEVIATION1 5.00000000000000000000e+00 FSK_SOURCE1 Internal FSK_RATE1 5.00000000000000000000e+01 FSK_HOP_FREQUENCY1 1.00000000000000000000e+06 SWEEP_START1 1.00000000000000000000e+05 SWEEP_STOP1 1.00000000000000000000e+06 SWEEP_CENTER1 5.50000000000000000000e+05 SWEEP_SPAN1 9.00000000000000000000e+05 SWEEP_START_STOP_OR_CENTER_SPAN1 StartStop SWEEP_TIME1 1.00000000000000002082e-02 SWEEP_RETURN_TIME1 1.00000000000000002082e-03 SWEEP_HOLD_TIME1 0.00000000000000000000e+00 SWEEP_TYPE1 Linear SWEEP_MODE1 Repeat BURST_DELAY1 0.00000000000000000000e+00 BURST_IDLE_STATE1 StartPoint RTWM_CABLE_DELAY1 5.23999999999999927584e-09 BURST_COUNT2 5.00000000000000000000e+00 BURST_MODE2 Triggered FREQUENCY_CONCURRENT2 Off FUNCTION2 Sine FUNCTION_FILE2 "" VOLTAGE_CONCURRENT2 Off LOAD_IMPEDANCE2 5.00000000000000000000e+01 AMPLITUDE_UNIT2 Vpp AMPLITUDE_VPP2 1.00000000000000000000e+00 AMPLITUDE_VRMS2 3.53553390593273730858e-01 AMPLITUDE_DBM2 3.97940008672037537352e+00 OFFSET2 0.00000000000000000000e+00 HIGH_LEVEL2 5.00000000000000000000e-01 LOW_LEVEL2 -5.00000000000000000000e-01 AMPLITUDE_OR_LEVEL2 Amplitude HIGH_LIMIT2 2.50000000000000000000e+00 LOW_LIMIT2 -2.50000000000000000000e+00 INVERT2 Off NOISE_ADD2 Off NOISE_LEVEL2 1.00000000000000000000e+01 PULSE_WIDTH2 4.99999999999999977374e-07 PULSE_DUTY2 5.00000000000000000000e+01 PULSE_WIDTH_OR_DUTY2 Duty PULSE_LEADING_EDGE2 2.00000000000000012456e-09 PULSE_TRAILING_EDGE2 2.00000000000000012456e-09 RAMP_SYMMETRY2 5.00000000000000000000e+01 NOISE_SIGMA2 2.00000000000000011102e-01 FREQUENCY2 1.00000000000000000000e+06 PERIOD2 9.99999999999999954748e-07 FREQUENCY_OR_PERIOD2 Frequency PHASE2 0.00000000000000000000e+00 LEAD_DELAY2 0.00000000000000000000e+00 PHASE_CONCURRENT2 Off RUN_MODE2 Continuous MODULATION_TYPE2 AM AM_SOURCE2 Internal AM_SHAPE2 Sine AM_SHAPE_FILE2 "" AM_FREQUENCY2 1.00000000000000000000e+04 AM_DEPTH2 5.00000000000000000000e+01 FM_SOURCE2 Internal FM_SHAPE2 Sine FM_SHAPE_FILE2 "" FM_FREQUENCY2 1.00000000000000000000e+04 FM_DEVIATION2 1.00000000000000000000e+06 PM_SOURCE2 Internal PM_SHAPE2 Sine PM_SHAPE_FILE2 "" PM_FREQUENCY2 1.00000000000000000000e+04 PM_DEVIATION2 9.00000000000000000000e+01 PWM_SOURCE2 Internal PWM_SHAPE2 Sine PWM_SHAPE_FILE2 "" PWM_FREQUENCY2 1.00000000000000000000e+04 PWM_DEVIATION2 5.00000000000000000000e+00 FSK_SOURCE2 Internal FSK_RATE2 5.00000000000000000000e+01 FSK_HOP_FREQUENCY2 1.00000000000000000000e+06 SWEEP_START2 1.00000000000000000000e+05 SWEEP_STOP2 1.00000000000000000000e+06 SWEEP_CENTER2 5.50000000000000000000e+05 SWEEP_SPAN2 9.00000000000000000000e+05 SWEEP_START_STOP_OR_CENTER_SPAN2 StartStop SWEEP_TIME2 1.00000000000000002082e-02 SWEEP_RETURN_TIME2 1.00000000000000002082e-03 SWEEP_HOLD_TIME2 0.00000000000000000000e+00 SWEEP_TYPE2 Linear SWEEP_MODE2 Repeat BURST_DELAY2 0.00000000000000000000e+00 BURST_IDLE_STATE2 StartPoint RTWM_CABLE_DELAY2 0.00000000000000000000e+00
Hello,
The example code is working as expected.
The AM263x Launchpad has 0.1µF capacitor to ground at the ADCx_AINy boosterpack pin. This is parallel to the load applied by the function generator and results in a LPF response that is likely attenuating signals in the 100KHz range as shown.
Best Regards,
Zackary Fleenor