Part Number: TMS570LC4357
Other Parts Discussed in Thread: HALCOGEN
Hi,
I am using a Hercules Safety MCU Development Kit TMS570.
I am unable to receive messages sent from Peak CAN. I am able to transmit messages.
When trying to receive messages, I see below errors in ES Register. LEC changes between 2 and 1 during debug session.

I am using STANDARD CAN and sending the below message from PCAN.

The NewDat bit in IF2MCTL never becomes one, even when new messages are being sent from PCAN.

I have checked the acceptance filtering settings and the mask is set to 0x1FFFFFFF to accept all messages.
I am using a baud rate of 1Mbps on both ends; software and PCAN. On PCAN when I turn on periodic sending of messages, the bus state changes to BUS HEAVY and then to BUS OFF.
As transmit is working as expected, I believe the wiring is correct.
Could you please suggest what could be causing the errors?
Regards,
Rashmitha