Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C1294NCPDT: Ethernet firmware update

Part Number: TM4C1294NCPDT
Other Parts Discussed in Thread: EK-TM4C1294XL

i want to update the firmware using ethernet i found this 

but i have some question why we need boot_demo_emac and why the boot_emac_flash is not enough and what happen when i load the boot_emac_flash and boot_demo_emac and i want to load another application what happen to boot_demo_emac would it still exist or the bootloader write the new code on it
  • So what is your question? You just post a link to another post. If you want to use Ethernet for firmware update then there are examples in TivaWare SDK. 

    You will use C:\ti\TivaWare_C_Series-2.2.0.295\examples\boards\ek-tm4c1294xl\boot_emac_flash as the example bootloader and

    C:\ti\TivaWare_C_Series-2.2.0.295\examples\boards\ek-tm4c1294xl\boot_demo_emac_flash as the example firmware. 

    As Explained in your referred post, below are the steps to be taken. 

    Step1: Run the enet_lwip or enet_io to obtain the IP address.  On the terminal window you should see the IP address printed out. Record this address. 

     Step2: Load the boot_emac_flash via the JTAG interface using CCS. This is the bootloader to be loaded at 0x0. 

     Step 3. Bring up the LM flash programmer. See below image. Provide the IP address that you just record in step 1 and enter the IP address and also the MAC address. If you are using the LaunchPad, the MAC address is shown on the sticker on the back of the board. 

    Your PC will be your TFTP server as well as a BootP server to transfer the program image to the MCU (the client). You need to inform the BootP server for the MCU’s IP address and its MAC address. This is how a BootP server works. Unlike a DHCP server, the MAC address and its associated IP address must be manually entered and known ahead of time because BootP is static in nature. This is why we enter them in the configuration tab. However, we don’t know what IP address to enter. We cannot enter any arbitrary address that might interfere with other IP address in the network.

    This is the reason we must first run a different Ethernet example such as enet_lwip. The enet_lwip will send the DHCP request. After the IP address is acquired we will just record the IP address value for reuse in boot_emac_flash. The IP address acquired by running enet_lwip shows 10.219.14.138 in my image. Note your address will be different from mine. The reason we can use this address is that the DHCP IP address is leased for some hours. The address we acquired by running the enet_lwip will be good for a few hours.

    Step 4. Go to the Program tab. Provide the path to the application image which is the boot_demo_emac_flash.bin. This TvaWare example was already llinked to 0x4000. DO NOT change it. You can change to wherever you like in the future. But until you get the example working, do NOT change anything. 

     Step 5. if the boot_emac_flash in step 2 is still halted in CCS, you can run it now. 

     Step 6. After the boot_emac_flash is run, you can hit the Program button in the above image.

     Step 7. Suppose everything went smoothly and the boot_demo_emac_flash application was programmed and if you want to debug it, you can load the symbol by going to Run->Load->Load Symbols. The symbol is contained in the boot_demo_emac_flash.out. Note it is the .out file. Do load symbols, not to be confused with Load program. 

    I will suggest you use WireShark to view the traffic between the MCU and the TFTP/BOOTP server. Below is what you should see. The MCU will send BOOTP request to the PC and after the handshake the TFTP sever sends the program image (boot_demo_emac_flash.bin) to the MCU via the Ethernet interface.

  • i have some question why we need boot_demo_emac and why the boot_emac_flash is not enough and what happen when i load the boot_emac_flash and boot_demo_emac and i want to load another application what happen to boot_demo_emac would it still exist or the bootloader write the new code on it