This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP-MSPM0G3507: Data corruption when using five ADC channels + single DMA Channel

Part Number: LP-MSPM0G3507

Tool/software:

Hello TI,

I configure the ADC0 for 5 different channels (for different pin) , and I got the example code for single channel ADC with DMA , but now we are trying to get all 5 ADC channel data from DMA but as I try the same we are getting garbage value ,

I found the below example code on the e2e which is similar as my counsion , but in that there two ADC (adc0 and adc1 is used )  instead of adc0 or adc1 for to different channels,

Can you please tell whether it is possible ? then please provide me the example code for the same, 

whether it is possible to configure multiple ADC0 channel with single DMA ? 

if not then please tell me how to configure multiple DMA with ADC0 with 5 different channels ?

best regard's 

adc_sim_dma_example (1).zip