Part Number: TM4C1290NCPDT
Tool/software:
Hello,
I have read the ROM_VERSION out of the ROM table and found 769. How can I translate this to the #define value that rom.h uses?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TM4C1290NCPDT
Tool/software:
Hello,
I have read the ROM_VERSION out of the ROM table and found 769. How can I translate this to the #define value that rom.h uses?
There is no need to know the ROM version. The ROM code is permanently programmed to the ROM memory during silicon fabrication. It may be more than 10 years since ithe code was frozen. What we recommend customers is to call MAP_xyz instead of ROM_xyz directly. Some of the APIs in ROM are deprecated. Calling MAP_xyz instead will result in calling ROM_xyz if the API in the ROM is still valid or otherwise will call xyz which is part of the library in the driverlib.lib. In your CCS project, you just need to define which device and which silicon version you have.
Refer to the below description.
34.3 Mapped ROM CallsWhen code is intended to be shared between projects, and some of the projects run on devices witha ROM and some run on devices without a ROM, it is convenient to have the code automaticallycall the ROM or the flash version of the API without having #ifdef-s in the code. rom_map.hprovides an automatic mapping feature for accessing the ROM. Similar to the ROM_Function()APIs provided by rom.h, a set of MAP_Function() APIs are provided. If the function is available inROM, MAP_Function() simply calls ROM_Function(); otherwise it calls Function().In order to use the mapped ROM calls, the following steps must be performed:Follow the above steps for including and using driverlib/rom.h.Include driverlib/rom_map.h.Continuing the above example, call MAP_GPIODirModeSet() in the source code.As in the direct ROM call method, the choice of calling ROM versus the flash version is made atcompile-time. The only APIs that are provided via the ROM mapping feature are ones that areavailable in the ROM, which is not every API available in the peripheral driver library.The following is an example of calling a function in shared code, where the device in question isdefined in the project file:
#include "driverlib/rom.h"#include "driverlib/rom_map.h"#include "driverlib/systick.h"voidSetupSysTick(void){MAP_SysTickPeriodSet(0x1000);Map_SysTickEnable();}When built for a device that does not have a ROM, this example is equivalent to:#include "driverlib/systick.h"voidSetupSysTick(void){SysTickPeriodSet(0x1000);SysTickEnable();}When built for a device that has a ROM, however, this example is equivalent to:#include "driverlib/rom.h"#include "driverlib/systick.h"voidSetupSysTick(void){ROM_SysTickPeriodSet(0x1000);ROM_SysTickEnable();
Thank you, I will use the MAP version for this portability. I suppose my question should have been how do I find which silicon version I am using? Currently I defined
Hi Sam,
#define TARGET_IS_TM4C129_RA2
This is correct.
There are two methods to do this. You can read the Device ID register. See below. You can also visually look at the device marking on the IC.