Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MCU-PLUS-SDK-AM263X: AM263P4: GPIO Configuration and VIM interrupts

Part Number: MCU-PLUS-SDK-AM263X
Other Parts Discussed in Thread: AM263P4

Tool/software:

Hello All,

1. Is the info provided in [FAQ] MCU-PLUS-SDK-AM263X: Configuring GPIO Interrupts - Arm-based microcontrollers forum - Arm-based microcontrollers - TI E2E support forums relevant to AM263P4 device as well?

2. VIM0 is connected to R50_0.  4 GPIO INT_XBARs can be routed to VIM_0 and hence to the R50_0 core. Does this mean we cannot have more than 4 GPIO ISR for each core? 

3. Please provide an example project with more than 1 gpio input interrupts. The example in sdk "gpio_input_interrupt example" uses a bank example.

Thanks,

Arjun