Part Number: AM2434
Tool/software:
#1. What is mean of the CAUTION Notes? only as a Digital Windowed Watchdog? can only be Watchdog?

#2. What is mean of Real time interrupt functionality, different with interrupt functionality?

#3. How to understand not support Periodic interrupt? can't auto reload period value?
#4. About the time out interrupt, When it trigger interrupt in different window size?

#5. Take 100 Window, When it generate interrupt, then how about 50%?

#6. in my customer use case, configured as 1000ms interrupt interval, but it is about 754ms interval from test result.



#6. Also captured RTI8 registers if needed, I checked not find big problem, just the period is (2+1)*2^13/25MHz, which is about 960ms.